imx8qxpmek use uuu to burn uboot with M4.bin fail

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx8qxpmek use uuu to burn uboot with M4.bin fail

3,895件の閲覧回数
475143463
Contributor III

version

uboot:2018.03

I use imx-mkimage to build flash.bin with flash_linux_m4.

After build,I use uuu to burn flash.bin into imx8qxpmek.

But, it is err.

The log is as follow:

U-Boot SPL 2018.03-imx_v2018.03_4.14.98_2.0.0_ga+g87a19df (Dec 15 2019 - 04:58:35 +0000)
Normal Boot
Trying to boot from USB SDP
1 setufp mode 0
1 cdns3_uboot_initmode 0
SDP: initialize...
SDP: handle requests...
Downloading file of size 1009664 to 0x80400000... done
Jumping to header at 0x80400000
Header Tag is not an IMX image
Found header at 0x80400000
U

U-Boot 2018.03 (Dec 19 2019 - 14:18:31 +0800)

CPU: Freescale i.MX8QXP revB A35 at 1200 MHz at 24C
Model: Freescale i.MX8QXP MEK
Board: iMX8QXP MEK
Boot: USB
DRAM: 2.8 GiB
imx_vservice_connect: Timeout to connect peer, -110
VService: Connection is failed, ret -110
virt_i2c: Faild to setup vservice
imx_vservice_connect: Timeout to connect peer, -110
VService: Connection is failed, ret -110
virt_i2c: Faild to setup vservice
imx_vservice_connect: Timeout to connect peer, -110
VService: Connection is failed, ret -110
virt_i2c: Faild to setup vservice
setup_typec lookup gpio@1a_7 failed ret = -19
MMC: FSL_SDHC: 0, FSL_SDHC: 1
Loading Environment from MMC... MMC: no card present
*** Warning - No block device, using default environment

Failed (-5)
[pcie_ctrlb_sata_phy_init_rc] LNK DOWN 8600000
In: serial
Out: serial
Err: serial

BuildInfo:
- SCFW f83a2bed, SECO-FW 92ef1143, IMX-MKIMAGE dd023400, ATF 1cb68fa
- U-Boot 2018.03

MMC: no card present
Detect USB boot. Will enter fastboot mode!
Net:
Warning: ethernet@5b040000 using MAC address from ROM
eth0: ethernet@5b040000 [PRIME]
Warning: ethernet@5b050000 (eth1) using random MAC address - ba:42:db:0f:7c:21
, eth1: ethernet@5b050000
Fastboot: Normal
Boot from USB for mfgtools
Use default environment for mfgtools
Run bootcmd_mfg: run mfgtool_args;if iminfo ${initrd_addr}; then if test ${tee} = yes; then bootm ${tee_addr} ${initrd_addr} ${fdt_addr}; else booti ${loadaddr} ${initrd_addr} ${fdt_addr}; fi; else echo "Run fastboot ..."; fastboot 0; fi;
Hit any key to stop autoboot: 0

## Checking Image at 83100000 ...
Legacy image found
Image Name: fsl-image-mfgtool-initramfs-imx8
Image Type: AArch64 Linux RAMDisk Image (uncompressed)
Data Size: 10798591 Bytes = 10.3 MiB
Load Address: 00000000
Entry Point: 00000000
Verifying Checksum ... Bad Data CRC
Run fastboot ...
dev_get_parent_platdata: null device
"Synchronous Abort" handler, esr 0x96000007
elr: 0000000080045720 lr : 0000000080052358 (reloc)
elr: 0000000087e9b720 lr : 0000000087ea8358
x0 : 0000000000000000 x1 : 0000000000000000
x2 : 000000000000000a x3 : 000000005a060014
x4 : 00000000ffffffff x5 : 0000000000000000
x6 : 0000000000000000 x7 : 0000000000000003
x8 : 0000000000001fc0 x9 : 0000000000000008
x10: 00000000ffffffd0 x11: 0000000085668208
x12: 0000000000001fbe x13: 0000000000000011
x14: 0000000000000001 x15: 0000000000000008
x16: 0000000000002080 x17: 0000000000000000
x18: 0000000085673da8 x19: 0000000000000000
x20: 0000000000000001 x21: 0000000085667dcf
x22: 0000000000000000 x23: 000000000000001d
x24: 0000000000000002 x25: 0000000000000001
x26: 0000000000000000 x27: 0000000000000000
x28: 00000000856b9150 x29: 0000000085667d00

Resetting CPU ...

resetting ...

Using imx8qxpmek at first time, could you give me some advice?

タグ(1)
0 件の賞賛
返信
4 返答(返信)

2,506件の閲覧回数
_angelo_
Contributor III

As often happen, NXP replies posting manual links. Sorry, honestly, this is not useful at all. I have this same issue, will post the solution, soon, hopefully.

0 件の賞賛
返信

3,591件の閲覧回数
josehdz
Contributor I

Hi.

I have the same issue, How can this be fixed?

0 件の賞賛
返信

3,591件の閲覧回数
189659318
Contributor I

Hi 一笑 独孤 

I also met the same problem. How did you solve it later?

0 件の賞賛
返信

3,591件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi 一笑 独孤 

if you are using board first time may be relevant first to look at

Get Started with the MCIMX8QXP-CPU | NXP 

Documentation

i.MX 8QuadXPlus Multisensory Enablement Kit | NXP 

Demo Images

i.MX Software and Development Tools | NXP 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信