code:
#define DSRC_PRI_RSTn IMX_GPIO_NR(4, 22)
#define DSRC_SEC_RSTn IMX_GPIO_NR(2, 3)
static iomux_cfg_t dsrc_pads[] = {
SC_P_USDHC1_CD_B | MUX_MODE_ALT(4) | MUX_PAD_CTRL(UART_PAD_CTRL),
SC_P_SCU_GPIO0_00 | MUX_MODE_ALT(4) | MUX_PAD_CTRL(UART_PAD_CTRL),
};
static void dsrc_init(void)
{
imx8_iomux_setup_multiple_pads(dsrc_pads, ARRAY_SIZE(dsrc_pads));
int ret=gpio_request(DSRC_PRI_RSTn, "DSRC_PRI_RSTn");printf("%s lookup DSRC_PRI_RSTn failed ret = %d\n", __func__, ret);
gpio_direction_output(DSRC_PRI_RSTn, 0);
mdelay(100);
gpio_set_value(DSRC_PRI_RSTn, 1);
gpio_free(DSRC_PRI_RSTn);
mdelay(100);
ret=gpio_request(DSRC_SEC_RSTn, "DSRC_SEC_RSTn");printf("%s lookup DSRC_SEC_RSTn failed ret = %d\n", __func__, ret);
gpio_direction_output(DSRC_SEC_RSTn, 0);
mdelay(100);
gpio_set_value(DSRC_SEC_RSTn, 1);
gpio_free(DSRC_SEC_RSTn);
}
test log :
U-Boot SPL 2020.04-4.14.98-2.3.1+gc2adcb7 (Feb 03 2021 - 09:38:26 +0000)
Normal Boot
WDT: Not found!
Trying to boot from SPI
Load image from QSPI 0x53400
U
U-Boot 2020.04-4.14.98-2.3.1+gc2adcb7 (Feb 03 2021 - 09:38:26 +0000) (TCU V0.604)
CPU: NXP i.MX8QXP RevC A35 at 1200 MHz at 48C
Model: NXP i.MX8QXP MEK
Board: iMX8QXP MEK
BuildInfo:
- SCFW 0d54291f, SECO-FW f449a0d2, IMX-MKIMAGE d7f9440d, ATF bb209a0
- U-Boot 2020.04-4.14.98-2.3.1+gc2adcb7
Boot: FLEXSPI
DRAM: 2 GiB
dsrc_init lookup DSRC_PRI_RSTn failed ret = 3
dsrc_init lookup DSRC_SEC_RSTn failed ret = 3
MMC: FSL_SDHC: 0, FSL_SDHC: 1
Loading Environment from SPI Flash... SF: Detected mt35xu512aba with page size 256 Bytes, erase size 128 KiB, total 64 MiB
OK
In: serial
Out: serial
Err: serial
Net:
Warning: ethernet@5b040000 (eth0) using random MAC address - fe:e9:f2:f4:90:50
eth0: ethernet@5b040000 [PRIME]
Warning: ethernet@5b050000 (euh1) using random MAC address - c2:2d:e4:d8:ca:d9
, eth1: ethernet@5b050000
Fastboot: Normal
Normal Boot
Hit any key to stop autoboot: 0
GPIO2_3 has not been used on dts.
opend enable CONFIG_USB_TCPC=y ,
tepy c GPIO is return 3 .
test log:
U-Boot 2020.04-4.14.98-2.3.1+gc2adcb7 (Feb 03 2021 - 09:29:02 +0000) (TCU V0.604)
CPU: NXP i.MX8QXP RevC A35 at 1200 MHz at 49C
Model: NXP i.MX8QXP MEK
Board: iMX8QXP MEK
BuildInfo:
- SCFW 0d54291f, SECO-FW f449a0d2, IMX-MKIMAGE d7f9440d, ATF bb209a0
- U-Boot 2020.04-4.14.98-2.3.1+gc2adcb7
Boot: USB
DRAM: 2 GiB
setup_typec lookup GPIO5_9 failed ret = 3
dsrc_init lookup DSRC_PRI_RSTn failed ret = 3
dsrc_init lookup DSRC_SEC_RSTn failed ret = 3
Have you tested it? Can you test it on the development board。
Hi grayli_wang
one can try to debug it using AN12631
Normal and Secure Debug for i.MX8/8X Family of Applications Processors
Best regards
igor