imx8qxp sai0 vs sai1

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
609件の閲覧回数
petero5
Contributor III

Hi

Noticed in IMX8DQXPRM.pdf Table 16-6. SAI Instance Configuration, the Use Case column has:
SAI0 - BT
SAI1 - External Audio CODEC/Processor

What is the significance of the Use Case please?
Is there any practical difference between sai0 and sai1?
Is there any reason not to use sai0 with External Audio CODEC/Processor?
Or is it just a suggestion/convention?

Thank you
-- Peter

ラベル(2)
0 件の賞賛
返信
1 解決策
567件の閲覧回数
JorgeCas
NXP TechSupport
NXP TechSupport

Hello,

1. The use case is the configuration for the audio subsystem.

2. On hardware perspective SAI0 and SAI1 have the same features:

- Tx/Rx Data Lines: 1/1.

- Tx FIFO Depth: 64/64.

- Pins: 6.

3. There is no documentation to not use SAI0 with External Audio CODEC/Processor, from hardware perspective have the same features.

4. By default, it seems that is a convention because there are some posts on NXP community were customers tried to add CODECs on other SAI ports with the same issue and they used patches to initialize the ALSA device.

Here an example.

Best regards.

元の投稿で解決策を見る

2 返答(返信)
568件の閲覧回数
JorgeCas
NXP TechSupport
NXP TechSupport

Hello,

1. The use case is the configuration for the audio subsystem.

2. On hardware perspective SAI0 and SAI1 have the same features:

- Tx/Rx Data Lines: 1/1.

- Tx FIFO Depth: 64/64.

- Pins: 6.

3. There is no documentation to not use SAI0 with External Audio CODEC/Processor, from hardware perspective have the same features.

4. By default, it seems that is a convention because there are some posts on NXP community were customers tried to add CODECs on other SAI ports with the same issue and they used patches to initialize the ALSA device.

Here an example.

Best regards.

548件の閲覧回数
petero5
Contributor III
Thank you!