imx8qxp-mek uuu fail

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx8qxp-mek uuu fail

Jump to solution
10,003 Views
475143463
Contributor III

hi sir,

After I got bootloader(2018.03-r0) and kernel(4.14.98-r0) from yocto,I also successfully compiled the BootLoader using imx8qxp_mek_defconfig and generated u-boot.bin.

Next, I use the cmd-command line on win10 to execute “uuu.exe SDPS: boot-f u-boot.bin”. But it was a failure.

The error message is as follows:

uuu (Universal Update Utility) for nxp imx chips -- libuuu_1.3.102-0-gb078bd0
Success 0    Failure 1

1:513    1/ 1 [HID(W):LIBUSB_ERROR_IO                ] SDPS: boot -f u-boot.bin
Error: HID(W):LIBUSB_ERROR_IO
Now, I have no idea to solve it, can you give some advice?
0 Kudos
Reply
1 Solution
9,239 Views
475143463
Contributor III

Thank you Mr Xie,

I am so sorry about this issue.

I forgot to use imx-mkimage tool to add some bins(spl,cswf,..etc) into flash.bin. so it can't bootup.

Now it is ok.

But, I can't start M4.bin during bootloader startup.

can you give me some suggests or guidance document  to achieve it?

View solution in original post

0 Kudos
Reply
7 Replies
9,238 Views
joanxie
NXP TechSupport
NXP TechSupport

did you change anything in uboot? if no, you can try to use demo uboot image to replace your own uboot.bin, you can use like "imx-boot-imx8qxpmek-sd.bin-flash" to replace your own uboot.bin

0 Kudos
Reply
9,239 Views
475143463
Contributor III

Thank you Mr Xie.

This way has been tested, it can be.

But in the future,I need change BootLoader to match my hardware.

Now, I can compile it with default-config file named imx8qxp_mek_defconfig.
But after compiled,it can not be burn into development board and uuu show this issue.

so,I have no idea to check this issue.

Can you give me some suggests?

0 Kudos
Reply
9,239 Views
joanxie
NXP TechSupport
NXP TechSupport

try to build uboot with the commands like below:

"bitbake -c clean u-boot-imx

bitbake -c compile -f u-boot-imx

bitbake -f u-boot-imx“

0 Kudos
Reply
9,240 Views
475143463
Contributor III

Thank you Mr Xie,

I am so sorry about this issue.

I forgot to use imx-mkimage tool to add some bins(spl,cswf,..etc) into flash.bin. so it can't bootup.

Now it is ok.

But, I can't start M4.bin during bootloader startup.

can you give me some suggests or guidance document  to achieve it?

0 Kudos
Reply
8,901 Views
SerdarKantarci
Contributor I

Hello,

I have the same problem.

I could boot an android image on the eMMC but not a pre-built linux image.

How exactly did you use the imx-mkimage tool?

0 Kudos
Reply
9,239 Views
joanxie
NXP TechSupport
NXP TechSupport

you need to download specific m4 bin file to board by UUU tools.

0 Kudos
Reply
9,239 Views
475143463
Contributor III

Thank you Mr Xie,

But,what is specific m4 bin file ?

And, how can I get it.

Now,I got bootloader(2018.03) and kernel(4.14.98) through yocto with default config(UBOOT_CONFIG = "sd").

After I compiled bootloader,I build flash.bin through imx-mkimage using flash_spl.

flash.bin is ok.And it can be burn into imx8qxpmek and run.

But I build flash.bin with flash_linux_m4,bin file is not good running.

and the err log is as follow:

U-Boot SPL 2018.03-imx_v2018.03_4.14.98_2.0.0_ga+g87a19df (Dec 15 2019 - 04:58:35 +0000)
Normal Boot
Trying to boot from USB SDP
1 setufp mode 0
1 cdns3_uboot_initmode 0
SDP: initialize...
SDP: handle requests...
Downloading file of size 1009664 to 0x80400000... done
Jumping to header at 0x80400000
Header Tag is not an IMX image
Found header at 0x80400000
U

U-Boot 2018.03 (Dec 25 2019 - 10:17:44 +0800)

CPU: Freescale i.MX8QXP revB A35 at 1200 MHz at 18C
Model: Freescale i.MX8QXP MEK
Board: iMX8QXP MEK
Boot: USB
DRAM: 2.8 GiB
imx_vservice_connect: Timeout to connect peer, -110
VService: Connection is failed, ret -110
virt_i2c: Faild to setup vservice
imx_vservice_connect: Timeout to connect peer, -110
VService: Connection is failed, ret -110
virt_i2c: Faild to setup vservice
imx_vservice_connect: Timeout to connect peer, -110
VService: Connection is failed, ret -110
virt_i2c: Faild to setup vservice
setup_typec lookup gpio@1a_7 failed ret = -19
MMC: FSL_SDHC: 0, FSL_SDHC: 1
Loading Environment from MMC... MMC: no card present
*** Warning - No block device, using default environment

Failed (-5)
[pcie_ctrlb_sata_phy_init_rc] LNK DOWN 8600000
In: serial
Out: serial
Err: serial

BuildInfo:
- SCFW f83a2bed, SECO-FW 92ef1143, IMX-MKIMAGE dd023400, ATF 1cb68fa
- U-Boot 2018.03

MMC: no card present
Detect USB boot. Will enter fastboot mode!
Net:
Warning: ethernet@5b040000 using MAC address from ROM
eth0: ethernet@5b040000 [PRIME]
Warning: ethernet@5b050000 (eth1) using random MAC address - c2:c6:3a:cc:7a:c5
, eth1: ethernet@5b050000
Fastboot: Normal
Boot from USB for mfgtools
Use default environment for mfgtools
Run bootcmd_mfg: run mfgtool_args;if iminfo ${initrd_addr}; then if test ${tee} = yes; then bootm ${tee_addr} ${initrd_addr} ${fdt_addr}; else booti ${loadaddr} ${initrd_addr} ${fdt_addr}; fi; else echo "Run fastboot ..."; fastboot 0; fi;
Hit any key to stop autoboot: 0

## Checking Image at 83100000 ...
Legacy image found
Image Name: fsl-image-mfgtool-initramfs-imx8
Image Type: AArch64 Linux RAMDisk Image (uncompressed)
Data Size: 10798591 Bytes = 10.3 MiB
Load Address: 00000000
Entry Point: 00000000
Verifying Checksum ... Bad Data CRC
Run fastboot ...
dev_get_parent_platdata: null device
"Synchronous Abort" handler, esr 0x96000007
elr: 0000000080045720 lr : 0000000080052358 (reloc)
elr: 0000000087e9b720 lr : 0000000087ea8358
x0 : 0000000000000000 x1 : 0000000000000000
x2 : 000000000000000a x3 : 000000005a060014
x4 : 00000000ffffffff x5 : 0000000000000000
x6 : 0000000000000000 x7 : 0000000000000003
x8 : 0000000000001fc0 x9 : 0000000000000008
x10: 00000000ffffffd0 x11: 0000000085668208
x12: 0000000000001fbe x13: 0000000000000011
x14: 0000000000000001 x15: 0000000000000008
x16: 0000000000002080 x17: 0000000000000000
x18: 0000000085673da8 x19: 0000000000000000
x20: 0000000000000001 x21: 0000000085667dcf
x22: 0000000000000000 x23: 000000000000001d
x24: 0000000000000002 x25: 0000000000000001
x26: 0000000000000000 x27: 0000000000000000
x28: 00000000856b9150 x29: 0000000085667d00

Resetting CPU ...

resetting ...

can you give me some suggests or guidance document  to achieve it?

0 Kudos
Reply