Hi all,
looking on RM Rev. 0, 05/2020, page 773, "IOMUXD_COMP_CTL_GPIO_1V8_3V3_ENET_ENETB0" section. I cannot understand properly the RM, about how to use this register.
Not sure if i understand properly, is bit 4 (PSW_OVR) to be used to set all TX/RX lines level to work at 1.8/3.3 or 2.5V ?
Thanks
Solved! Go to Solution.
Hi @_angelo_,
PSW_OVR should be set to 0 for 1.8/3.3V logic operation.
Thanks & Regards,
Ritesh M Patel
Thanks for the support.
Hi @riteshmpatel ,
ok, so if my logic is at 1.8V, i shouldn't touch such registers. Correct ?
Hi @_angelo_,
PSW_OVR should be set to 0 for 1.8/3.3V logic operation.
Thanks & Regards,
Ritesh M Patel
Hi @_angelo_,
I hope you are doing well.
PSW_OVR is an override bit that enables using 2.5V with the compensation IO cell, which natively only supports 1.8V and 3.3V.
Thanks & Regards,
Ritesh M Patel