imx8qxp, help on IOMUXD_COMP_CTL_GPIO_1V8_3V3_ENET_ENETB0

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx8qxp, help on IOMUXD_COMP_CTL_GPIO_1V8_3V3_ENET_ENETB0

Jump to solution
639 Views
_angelo_
Contributor III

Hi all,

 

looking on RM Rev. 0, 05/2020, page 773, "IOMUXD_COMP_CTL_GPIO_1V8_3V3_ENET_ENETB0" section. I cannot understand properly the RM, about how to use this register.

Not sure if i understand properly, is bit 4 (PSW_OVR) to be used to set all TX/RX lines level to work at 1.8/3.3 or 2.5V ?

Thanks

0 Kudos
1 Solution
612 Views
riteshmpatel
NXP TechSupport
NXP TechSupport

Hi @_angelo_,

PSW_OVR should be set to 0 for 1.8/3.3V logic operation.

Thanks & Regards,
Ritesh M Patel

View solution in original post

0 Kudos
4 Replies
599 Views
_angelo_
Contributor III

Thanks for the support.

0 Kudos
622 Views
_angelo_
Contributor III

Hi @riteshmpatel ,

ok, so if my logic is at 1.8V, i shouldn't touch such registers. Correct ?

0 Kudos
613 Views
riteshmpatel
NXP TechSupport
NXP TechSupport

Hi @_angelo_,

PSW_OVR should be set to 0 for 1.8/3.3V logic operation.

Thanks & Regards,
Ritesh M Patel

0 Kudos
628 Views
riteshmpatel
NXP TechSupport
NXP TechSupport

Hi @_angelo_,

I hope you are doing well.

PSW_OVR is an override bit that enables using 2.5V with the compensation IO cell, which natively only supports 1.8V and 3.3V.

Thanks & Regards,
Ritesh M Patel

0 Kudos