imx8qxp hdmi not output for adv7535

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx8qxp hdmi not output for adv7535

1,556件の閲覧回数
weikeng-jimmy
Contributor III

Hi Sir,

My customer try to test HDMI output from ADV7535 bridge in imx8qxp-mek board. We use command "modetest -c" and get log as below

I set mode "56:1920x1080-60" can get color bar in the monitor , but monitor can't show color bar when change resolution to 1280x720-60 or 1024x768-60.

Why we can get EDID modes but can't show color bar?

BSP version : Yocto BSP 4.14.78

monitor: 

DELL -> P2415Q6

ACER -> CB280HK

log :
id encoder status name size (mm) modes encoders
56 0 connected HDMI-A-1 620x340 35 55
modes:
name refresh (Hz) hdisp hss hse htot vdisp vss vse vtot)
1920x1080 60 1920 2008 2052 2200 1080 1084 1089 1125 148500 flags: phsync, pvsync; type: driver
1920x1080 60 1920 2008 2052 2200 1080 1084 1089 1125 148352 flags: phsync, pvsync; type: driver
1920x1080 50 1920 2448 2492 2640 1080 1084 1089 1125 148500 flags: phsync, pvsync; type: driver
1920x1080 30 1920 2008 2052 2200 1080 1084 1089 1125 74250 flags: phsync, pvsync; type: driver
1920x1080 30 1920 2008 2052 2200 1080 1084 1089 1125 74176 flags: phsync, pvsync; type: driver
1920x1080 24 1920 2558 2602 2750 1080 1084 1089 1125 74250 flags: phsync, pvsync; type: driver
1920x1080 24 1920 2558 2602 2750 1080 1084 1089 1125 74176 flags: phsync, pvsync; type: driver
1680x1050 60 1680 1728 1760 1840 1050 1053 1059 1080 119000 flags: phsync, nvsync; type: driver
1280x1024 75 1280 1296 1440 1688 1024 1025 1028 1066 135000 flags: phsync, pvsync; type: driver
1280x1024 60 1280 1328 1440 1688 1024 1025 1028 1066 108000 flags: phsync, pvsync; type: driver
1440x900 60 1440 1488 1520 1600 900 903 909 926 88750 flags: phsync, nvsync; type: driver
1280x960 60 1280 1376 1488 1800 960 961 964 1000 108000 flags: phsync, pvsync; type: driver
1280x800 60 1280 1328 1360 1440 800 803 809 823 71000 flags: phsync, nvsync; type: driver
1152x864 75 1152 1216 1344 1600 864 865 868 900 108000 flags: phsync, pvsync; type: driver
1280x768 60 1280 1344 1472 1664 768 771 778 798 79500 flags: nhsync, pvsync; type: driver
1280x720 60 1280 1390 1430 1650 720 725 730 750 74250 flags: phsync, pvsync; type: driver
1280x720 60 1280 1390 1430 1650 720 725 730 750 74176 flags: phsync, pvsync; type: driver
1280x720 50 1280 1720 1760 1980 720 725 730 750 74250 flags: phsync, pvsync; type: driver
1024x768 75 1024 1040 1136 1312 768 769 772 800 78750 flags: phsync, pvsync; type: driver
1024x768 70 1024 1048 1184 1328 768 771 777 806 75000 flags: nhsync, nvsync; type: driver
1024x768 60 1024 1048 1184 1344 768 771 777 806 65000 flags: nhsync, nvsync; type: driver
832x624 75 832 864 928 1152 624 625 628 667 57284 flags: nhsync, nvsync; type: driver
800x600 75 800 816 896 1056 600 601 604 625 49500 flags: phsync, pvsync; type: driver
800x600 72 800 856 976 1040 600 637 643 666 50000 flags: phsync, pvsync; type: driver
800x600 60 800 840 968 1056 600 601 605 628 40000 flags: phsync, pvsync; type: driver
800x600 56 800 824 896 1024 600 601 603 625 36000 flags: phsync, pvsync; type: driver
720x576 50 720 732 796 864 576 581 586 625 27000 flags: nhsync, nvsync; type: driver
720x480 60 720 736 798 858 480 489 495 525 27027 flags: nhsync, nvsync; type: driver
720x480 60 720 736 798 858 480 489 495 525 27000 flags: nhsync, nvsync; type: driver
640x480 75 640 656 720 840 480 481 484 500 31500 flags: nhsync, nvsync; type: driver
640x480 73 640 664 704 832 480 489 492 520 31500 flags: nhsync, nvsync; type: driver
640x480 67 640 704 768 864 480 483 486 525 30240 flags: nhsync, nvsync; type: driver
640x480 60 640 656 752 800 480 490 492 525 25200 flags: nhsync, nvsync; type: driver
640x480 60 640 656 752 800 480 490 492 525 25175 flags: nhsync, nvsync; type: driver
720x400 70 720 738 846 900 400 412 414 449 28320 flags: nhsync, pvsync; type: driver

ラベル(2)
タグ(2)
0 件の賞賛
返信
1 返信

1,246件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi JIMMY

BSP 4.14.78 is very old release, please try with latest L4.14.98 or L4.19.35

which implemented many improvements:

linux-imx - i.MX Linux kernel 

linux-imx - i.MX Linux kernel 

Linux  Documentation
i.MX Software | NXP 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信