Hi
I'm using imx8qxp, Yocto 3.0.
The same image boot normally on the SD card, but after burning to EMMC, there is no log output in the uboot phase, and the kernel phase is normal.
I feel this phenomenon is so strange and I don't have any ideas, so I'd like to ask if you have any good ideas
Hi Jimmychan:
Thank you for your reply.
We use our customized board.
Boot mode has been modified to boot from EMMC.
After starting from the SD card, we can successfully mount the EMMC, and the same content as the SD card can be seen in the EMMC.
Unplug the SD card, the EMMC boot normally, but there is no log output in the uboot phase.
Yes, there is no log output in the uboot phase, and the kernel phase is normal.