imx8qxp display passthru

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx8qxp display passthru

1,018 Views
minskey_guo
Contributor II

Hi, 

    imx8qxp has two LDBs and only one GPU.  Is it possible to allocate the GPU and one LDB to a VM (via drm/dri  driver),  and the other LDB to the second VM (via framebuffer driver ??).  so that both of the virtual machines have display output ?

thanks,

-minskey

0 Kudos
Reply
1 Reply

876 Views
igorpadykov
NXP Employee
NXP Employee

Hi Minskey

seems this is possible using resource partitioning through SCU and XRDC infrastructure.

For example almost every module description of i.MX8QXP Reference Manual has reference:

"Each of the peripherals, and local peripheral clock controls, and each
of the DMA channels can be uniquely assigned to different resource domains, security
domains, and virtual machines (VMs).
NOTE
The XRDC2 itself is only accessed by the System Controller via the DSC."

May be useful to look at presentation for resource partitioning on i.MX 8 Family

i.MX 8 Product Overview 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply