imx8qxp androidP 2.1.0 Car uuu flash issue

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

imx8qxp androidP 2.1.0 Car uuu flash issue

1,694 次查看
jiujinhong
Contributor IV

Hi,

when burnning androidP 2.1.0 car image into 8qxp board, it says below error. please give some advice. thanks.

U-Boot 2018.03 (May 22 2019 - 14:36:48 +0800)

CPU:   Freescale i.MX8QXP revB A35 at 1200 MHz at 47C
Model: Freescale i.MX8QXP MEK
Board: iMX8QXP MEK
Boot:  USB
DRAM:  3 GiB
Error reading output register
Error reading output register
Error reading output register
setup_typec lookup gpio@1a_7 failed ret = 3
MMC:   FSL_SDHC: 0, FSL_SDHC: 1
Loading Environment from MMC... MMC: no card present
*** Warning - No block device, using default environment

Failed (-5)
TX PLL is not locked.
In:    serial
Out:   serial
Err:   serial

 BuildInfo:
  - SCFW f83a2bed, SECO-FW 92ef1143, IMX-MKIMAGE dd023400, ATF a-20190
  - U-Boot 2018.03

Detect USB boot. Will enter fastboot mode!
Net:   No ethernet found.
MMC: no card present
Block device mmc 1 not supported
bcb_rw_block, get_block_size return 0
read_bootctl, bcb_rw_block read failed
read command failed
Fastboot: Normal
Boot from USB for uuu
Hit any key to stop autoboot:  0
dev_get_parent_platdata: null device
"Synchronous Abort" handler, esr 0x96000007
elr: 0000000080046728 lr : 0000000080053c30 (reloc)
elr: 00000000ffe89728 lr : 00000000ffe96c30
x0 : 0000000000000000 x1 : 0000000000000000
x2 : 000000000000000a x3 : 0000000000000001
x4 : 0000000000000020 x5 : 0000000000000000
x6 : 00000000ffffffd0 x7 : 00000000ffeed748
x8 : 00000000ffeed7c8 x9 : 0000000000000008
x10: 00000000ffee2228 x11: 000000000000000d
x12: 0000000000000006 x13: 0000000000017eeb
x14: 0000000000000000 x15: 00000000ffe64244
x16: 0000000000000000 x17: 0000000000000000
x18: 00000000fb260da8 x19: 0000000000000000
x20: 0000000000000001 x21: 00000000fb254e6f
x22: 0000000000000000 x23: 000000000000001d
x24: 0000000000000002 x25: 0000000000000000
x26: 0000000000000000 x27: 00000000fb26dc20
x28: 0000000000000000 x29: 00000000fb254da0

Resetting CPU ...

resetting ...

0 项奖励
3 回复数

1,051 次查看
igorpadykov
NXP Employee
NXP Employee

Hi jiu

what board used in the case, if this is custom board, image should be rebuilt

with new ddr settings found from ddr test. If this is MEK board, one can try other board

or try to run Linux Image from :

i.MX Software | NXP 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励

1,050 次查看
jiujinhong
Contributor IV

pastedImage_1.png

D:\project\IMX8\tools\uuu\mek_8q_image 的目录

2019/05/22  15:03    <DIR>          .
2019/05/22  15:03    <DIR>          ..
2019/05/22  14:47        50,331,648 boot.img
2019/05/22  15:03    <SYMLINK>      boot.img.link [boot.img]
2019/05/22  14:47         1,713,152 bootloader-imx8qxp.img
2019/05/22  15:03    <SYMLINK>      bootloader-imx8qxp.img.link [bootloader-imx8qxp.img]
2019/05/22  14:47         4,194,304 dtbo-imx8qxp.img
2019/05/22  15:03    <SYMLINK>      dtbo-imx8qxp.img.link [dtbo-imx8qxp.img]
2018/11/28  13:28           613,888 libusb-1.0.dll
2019/05/22  14:47             6,157 partition-table.bpt
2019/05/22  14:47            34,304 partition-table.img
2019/05/22  15:03    <SYMLINK>      partition-table.img.link [partition-table.img]
2019/05/22  14:47                36 rpmb_key_test.bin
2019/05/22  14:47           425,984 spl-imx8qxp.bin
2019/05/22  15:03    <SYMLINK>      spl-imx8qxp.bin.link [spl-imx8qxp.bin]
2019/05/22  14:47     1,227,727,104 system.img
2019/05/22  15:03    <SYMLINK>      system.img.link [system.img]
2019/05/22  14:47             1,032 testkey_public_rsa4096.bin
2019/05/22  14:47         1,038,336 u-boot-imx8qxp-mek-uuu.imx
2019/05/22  15:03    <SYMLINK>      u-boot-imx8qxp-mek-uuu.imx.link [u-boot-imx8qxp-mek-uuu.imx]
2019/05/22  13:17           935,936 uuu.exe
2019/05/22  15:03             1,021 uuu.lst
2019/05/22  14:47            25,361 uuu_imx_android_flash.bat
2019/05/22  14:47             4,096 vbmeta-imx8qxp.img
2019/05/22  15:03    <SYMLINK>      vbmeta-imx8qxp.img.link [vbmeta-imx8qxp.img]
2019/05/22  14:47        64,639,136 vendor.img
2019/05/22  15:03    <SYMLINK>      vendor.img.link [vendor.img]
              25 个文件  1,351,691,495 字节
               2 个目录 321,988,157,440 可用字节

D:\project\IMX8\tools\uuu\mek_8q_image>p

0 项奖励

1,051 次查看
jiujinhong
Contributor IV

U-Boot 2018.03 (May 22 2019 - 14:36:48 +0800)

CPU:   Freescale i.MX8QXP revB A35 at 1200 MHz at 47C
Model: Freescale i.MX8QXP MEK
Board: iMX8QXP MEK
Boot:  USB
DRAM:  3 GiB
Error reading output register
Error reading output register
Error reading output register
setup_typec lookup gpio@1a_7 failed ret = 3
MMC:   FSL_SDHC: 0, FSL_SDHC: 1
Loading Environment from MMC... MMC: no card present
*** Warning - No block device, using default environment

Failed (-5)
TX PLL is not locked.
In:    serial
Out:   serial
Err:   serial

 BuildInfo:
  - SCFW f83a2bed, SECO-FW 92ef1143, IMX-MKIMAGE dd023400, ATF a-20190
  - U-Boot 2018.03

Detect USB boot. Will enter fastboot mode!
Net:   No ethernet found.
MMC: no card present
Block device mmc 1 not supported
bcb_rw_block, get_block_size return 0
read_bootctl, bcb_rw_block read failed
read command failed
Fastboot: Normal
Boot from USB for uuu
Hit any key to stop autoboot:  0
dev_get_parent_platdata: null device
"Synchronous Abort" handler, esr 0x96000007
elr: 0000000080046728 lr : 0000000080053c30 (reloc)
elr: 00000000ffe89728 lr : 00000000ffe96c30
x0 : 0000000000000000 x1 : 0000000000000000
x2 : 000000000000000a x3 : 0000000000000001
x4 : 0000000000000020 x5 : 0000000000000000
x6 : 00000000ffffffd0 x7 : 00000000ffeed748
x8 : 00000000ffeed7c8 x9 : 0000000000000008
x10: 00000000ffee2228 x11: 000000000000000d
x12: 0000000000000006 x13: 0000000000017eeb
x14: 0000000000000000 x15: 00000000ffe64244
x16: 0000000000000000 x17: 0000000000000000
x18: 00000000fb260da8 x19: 0000000000000000
x20: 0000000000000001 x21: 00000000fb254e6f
x22: 0000000000000000 x23: 000000000000001d
x24: 0000000000000002 x25: 0000000000000000
x26: 0000000000000000 x27: 00000000fb26dc20
x28: 0000000000000000 x29: 00000000fb254da0

Resetting CPU ...

resetting ...


U-Boot 2018.03 (May 22 2019 - 14:36:48 +0800)

CPU:   Freescale i.MX8QXP revB A35 at 1200 MHz at 47C
Model: Freescale i.MX8QXP MEK
Board: iMX8QXP MEK
Boot:  USB
DRAM:  3 GiB
Error reading output register
Error reading output register
Error reading output register
setup_typec lookup gpio@1a_7 failed ret = 3
MMC:   FSL_SDHC: 0, FSL_SDHC: 1
Loading Environment from MMC... MMC: no card present
*** Warning - No block device, using default environment

Failed (-5)
TX PLL is not locked.
In:    serial
Out:   serial
Err:   serial

 BuildInfo:
  - SCFW f83a2bed, SECO-FW 92ef1143, IMX-MKIMAGE dd023400, ATF a-20190
  - U-Boot 2018.03

Detect USB boot. Will enter fastboot mode!
Net:   No ethernet found.
MMC: no card present
Block device mmc 1 not supported
bcb_rw_block, get_block_size return 0
read_bootctl, bcb_rw_block read failed
read command failed
Fastboot: Normal
Boot from USB for uuu
Hit any key to stop autoboot:  0
=>  mmc dev 1
MMC: no card present
=> mmc dev 0
switch to partitions #0, OK
mmc0(part 0) is current device
=> mmc info
Device: FSL_SDHC
Manufacturer ID: 13
OEM: 14e
Name: S0J57
Bus Speed: 200000000
Mode : HS400 (200MHz)
Rd Block Len: 512
MMC version 5.1
High Capacity: Yes
Capacity: 29.6 GiB
Bus Width: 8-bit DDR
Erase Group Size: 512 KiB
HC WP Group Size: 8 MiB
User Capacity: 29.6 GiB WRREL
Boot Capacity: 31.5 MiB ENH
RPMB Capacity: 4 MiB ENH
=>

0 项奖励