I am a little worried. The SDK I use is Q10.0.0_2.2.0_AUTO_SOURCE. The product I chose at the beginning is mek_8q-userdebug. I have implemented display, touch screen, wifi/Bluetooth.
I am now changing the product to mek_8q_car-userdebug. I reconfigured the device tree, but it cannot be displayed normally, and the i2c bus registration is not successful.
解決済! 解決策の投稿を見る。
I have solved this problem
We did not use extended I2C and extended IO chips. When M4 starts, it will perform LVDS display by default and use I2C to control extended IO. M4 will execute the LPI2C_MasterStop function.
Can't pick it out in the while.
The solution is to delete the code used to operate PCA9646PW and PCA9557PW.
if ((status & kLPI2C_MasterStopDetectFlag) && (status & kLPI2C_MasterTxReadyFlag))
{
LPI2C_MasterClearStatusFlags(base, kLPI2C_MasterStopDetectFlag);
break;
}
do you mean when build Q10.0.0_2.2.0_AUTO by command "lunch mek_8q-userdebug", everything is ok, but when you choose "lunch mek_8q_car-userdebug" to build the source code, the images you flash to the board, you couldn't display normally?
if yes, but according to the user guide, this bsp version only supports mek_8q_car-userdebug and mek_8q_car2-userdebug, how about use the demo images from nxp official website?
I use automotive-10.0.0_2.2.0_image_8qmek2.tar.gz. It is normal and the I2C bus will be created. But using automotive-10.0.0_2.2.0_image_8qmek.tar.gz, there is no i2c bus created.
I have solved this problem
We did not use extended I2C and extended IO chips. When M4 starts, it will perform LVDS display by default and use I2C to control extended IO. M4 will execute the LPI2C_MasterStop function.
Can't pick it out in the while.
The solution is to delete the code used to operate PCA9646PW and PCA9557PW.
if ((status & kLPI2C_MasterStopDetectFlag) && (status & kLPI2C_MasterTxReadyFlag))
{
LPI2C_MasterClearStatusFlags(base, kLPI2C_MasterStopDetectFlag);
break;
}
The PMIC I currently use is MC33PF8100A0ES.
The official website requires MC33PF8100CCES
I don't know if this has any effect?
thank you for your reply
Yes, I use a custom board, and the important parts are as consistent as possible, such as MIPI-DSI (DS90UB941/8), MIPI-CSI (NVP6324). There are some differences. M4_I2C0 is not used, and the debug ports of A core and M4 are separate.
During the startup of the board, there is no output from the debug port of M4.
Compare your [Com COM49] (2021-01-28_111250).log and confirm again that the i2c bus of the machine is not registered.
[115.922025] read descriptors
[115.924942] read strings
mek_8q:/ # i2cdetect -l
[116.961940] read descriptors
[116.964863] read strings
mek_8q:/ #
[118.005965] read descriptors
[118.008882] read strings