imx8qxp 使用uuu工具如何单独烧写rootfs到emmc

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx8qxp 使用uuu工具如何单独烧写rootfs到emmc

2,521 Views
353972149
Contributor I

imx8qxp 使用uuu工具如何单独烧写rootfs到emmc ?

现在我只能通过烧写sdcard整体去烧写uboot image 和rootfs,如何单独烧写rootfs到mmcblk0p2?

能不能提供一个脚本给我?

0 Kudos
Reply
1 Reply

1,552 Views
CarlosCasillas
NXP Employee
NXP Employee

Hi,

I’m afraid that i.MX8QXP is still on preproduction and no additional information/support could be provided yet. For further assistance, please contact with your Sales/FAE.

Just as hint, you could refer to the following Community thread, that provides additional UUU examples, and points to UUU documentation that could help you:

https://community.nxp.com/message/1176784 


Hope this will be useful for you.
Best regards!
/Carlos
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

-------------------------------------------------------------------------------

0 Kudos
Reply