[imx8qmmek][rpmsg][remoteproc] remoteproc and rpmsg fail.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

[imx8qmmek][rpmsg][remoteproc] remoteproc and rpmsg fail.

1,515 Views
WolsYang
Contributor IV

I am trying to do remoteproc and rpmsg with i.MX 8QMax MEK Linux Binary Demo files and i.MX Yocto Project User's Guide, Rev. LF5.10.72_2.2.0, 17 December 2021.

My M4 image is come from Demo files/imx_mcore_demos/imx8qm_m4_TCM_hello_world_m40.bin & 

i.MX8QM-MEK-MCUSDK/m4/boards/mekmimx8qm/multicore_examples/rpmsg_lite_str_echo_rtos/cm4_core0/armgcc/debug/rpmsg_lite_str_echo_rtos_imxcm4_m40.elf

And Linux image comming from Yocto version is 5.10.72-lts-5.10.y+ga68e31b63f86 :

 

$ DISTRO=fsl-imx-wayland MACHINE=imx8qmmek source  imx-setup-release.sh -b build
$ bitbake imx-image-full

 

===============================================================================

When I power on, M4 print hello world and keep go into Linux shell..

Then I do modprobe imx_rpmsg_tty and fail

 

root@imx8qmmek:~# modprobe imx_rpmsg_tty
modprobe: FATAL: Module imx_rpmsg_tty not found in directory /lib/modules/5.10.72-lts-5.10.y+ga68e31b63f86

 

Change M4 firmware through remotproc also fail 

 

root@imx8qmmek:~# cd /lib/firmware/
root@imx8qmmek:/lib/firmware# echo rpmsg_lite_str_echo_rtos_imxcm4_m40.elf > /sys/class/remoteproc/remoteproc0/firmware 
root@imx8qmmek:/lib/firmware# cat /sys/class/remoteproc/remoteproc0/firmware 
rpmsg_lite_str_echo_rtos_imxcm4_m40.elf
root@imx8qmmek:/lib/firmware# cat /sys/class/remoteproc/remoteproc0/state 
offline
root@imx8qmmek:/lib/firmware# echo start > /sys/class/remoteproc/remoteproc0/state 
[  869.481128] remoteproc remoteproc0: powering up imx-dsp-rproc
[  869.494189] remoteproc remoteproc0: Booting fw image rpmsg_lite_str_echo_rtos_imxcm4_m40.elf, size 512636
[  869.544564] remoteproc remoteproc0: Registered carveout doesn't fit da request
[  869.551943] remoteproc remoteproc0: Failed to process resources: -12
[  869.558636] remoteproc remoteproc0: Boot failed: -12
-sh: echo: write error: Cannot allocate memory

 

==============================================================================

This is dts I am use showing in uboot(u-boot => printenv).

 

fdt_file=imx8qm-mek-rpmsg.dtb

 

Also I check the kernel config, it is already turn on rpmsg:

 

root@imx8qmmek:/lib/firmware# uname -r
5.10.72-lts-5.10.y+ga68e31b63f86
root@imx8qmmek:/lib/firmware# zcat /proc/config.gz | grep -i rpmsg                                                                                                                                                 
CONFIG_KEYBOARD_RPMSG=y
CONFIG_GPIO_IMX_RPMSG=y
# CONFIG_REGULATOR_PF1550_RPMSG is not set
CONFIG_SND_SOC_FSL_RPMSG=y
CONFIG_SND_SOC_IMX_AUDIO_RPMSG=y
CONFIG_SND_SOC_IMX_PCM_RPMSG=y
CONFIG_SND_SOC_IMX_RPMSG=y
CONFIG_SND_SOC_RPMSG_WM8960=y
CONFIG_SND_SOC_RPMSG_WM8960_I2C=y
CONFIG_SND_SOC_RPMSG_AK4497=y
CONFIG_RTC_DRV_IMX_RPMSG=y
# CONFIG_CROS_EC_RPMSG is not set
# Rpmsg drivers
CONFIG_RPMSG=y
CONFIG_RPMSG_CHAR=y
CONFIG_RPMSG_CTRL=y
CONFIG_RPMSG_NS=y
CONFIG_RPMSG_QCOM_GLINK=y
CONFIG_RPMSG_QCOM_GLINK_RPM=y
CONFIG_RPMSG_VIRTIO=y
CONFIG_HAVE_IMX_RPMSG=y
CONFIG_IMX_RPMSG_PINGPONG=m
CONFIG_IMX_RPMSG_TTY=m
# end of Rpmsg drivers
CONFIG_RPMSG_LIFE_CYCLE=y

 

 

 

 

0 Kudos
1 Reply

1,491 Views
WolsYang
Contributor IV

To fix the missing imx_rpmsg_tty kernel module error :

Add this line to your layer.conf. 

 

IMAGE_INSTALL_append = "kernel-modules" 

 

I think kernel modules should install automatically, but now just add it and fix the problem : )

The remoteproc still falling hopefully got good news soon : (

 

 

0 Kudos