Hi igorpadykov,
Thanks.Gstreamer is already included, for I can use gplay command to play video below.But when I use qml mediaplayer to play video, it failed.
root@imx8qmmek:/run/media/mmcblk1p3/videos# gplay-1.0 car.avi
FSL_GPLAY2_01.00_LINUX build on May 20 2019 10:18:11
Set VideoSink imxvideoconvert_g2d ! queue ! waylandsink
Set TextSink fakesink
====== AIUR: 4.4.5 build on May 20 2019 10:17:54. ======
Core: AVI_PARSER_03.06.06 build on Feb 25 2019 02:36:36
file: /usr/lib/imx-mm/parser/lib_avi_parser_arm_elinux.so.3.1
------------------------
Track 00 [video_0] Enabled
Duration: 0:00:06.973633000
Language: und
Mime:
video/mpeg, systemstream=(boolean)false, parsed=(boolean)true, mpegversi
on=(int)4, width=(int)720, height=(int)720, framerate=(fraction)30000/1001, code
c_data=(buffer)000001b001000001b58913000001000000012000c48d8ba98516845a146300000
1b24c61766335372e3130322e313030
------------------------
------------------------
Track 01 [audio_0] Enabled
Duration: 0:00:07.000816000
Language: und
Mime:
audio/mpeg, mpegversion=(int)1, channels=(int)2, rate=(int)44100, bitrat
e=(int)0
------------------------
[ 71.896696] [VPU Decoder] firmware version is 1.3.1
====== BEEP: 4.4.5 build on May 20 2019 10:18:00. ======
Core: MP3 decoder Wrapper build on Jan 11 2018 10:20:25
file: /usr/lib/imx-mm/audio-codec/wrap/lib_mp3d_wrap_arm_elinux.so.3
CODEC: BLN_MAD-MMCODECS_MP3D_ARM_02.13.01_ARMV8 build on Jan 11 2018 10:05:45.
===!!! Current pulsesink device is auto_null !!!===
[Stop (No Repeated)][Vol=1.0][00:00:00/00:00:07]=========== fsl_player_play() ==
================
FSL_GPLAY2_01.00_LINUX build on May 20 2019 10:18:11
[h]display the operation Help
[p]Play
[s]Stop
[e]Seek
[a]Pause when playing, play when paused
[v]Volume
[m]Switch to mute or not
[>]Play next file
[<]Play previous file
[r]Switch to repeated mode or not
[u]Select the video track
[d]Select the audio track
[b]Select the subtitle track
[f]Set full screen
[z]resize the width and height
[t]Rotate
[c]Setting play rate
[i]Display the metadata
[x]eXit
State changed: buffering
State changed: playing
[Playing (No Repeated)][Vol=1.0][00:00:00/00:00:07]
[Playing (No Repeated)][Vol=1.0][00:00:00/00:00:07]
[Playing (No Repeated)][Vol=1.0][00:00:00/00:00:07]
[Playing (No Repeated)][Vol=1.0][00:00:01/00:00:07]
[Playing (No Repeated)][Vol=1.0][00:00:02/00:00:07]
[Playing (No Repeated)][Vol=1.0][00:00:03/00:00:07]
[Playing (No Repeated)][Vol=1.0][00:00:04/00:00:07]
[Playing (No Repeated)][Vol=1.0][00:00:05/00:00:07]
[Playing (No Repeated)][Vol=1.0][00:00:06/00:00:07]EOS Found
getNextItem No next item!
No more media file, exit gplay!
State changed: stopped
FSL_PLAYER_UI_MSG_EXIT
Total showed frames (203), playing for (0:00:06.974473000), fps (29.106).
Exit display thread
fsl_player_deinit