imx8qm surround view question.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx8qm surround view question.

Jump to solution
3,079 Views
kangmw086
Contributor III

I referred to the following documents of NXP.

(Surround View Application, User’s Guide, Rev. 1, 07/2018)

I purchased and installed all the components of the document.

i.mx8qm mek board u-boot message.

U-Boot 2018.03-4.14.98-2.3.3+gc20c44482b (Jan 10 2022 - 08:39:51 +0000)

CPU: Freescale i.MX8QM revB A53 at 1200 MHz at 32C
Model: Freescale i.MX8QM MEK
Board: iMX8QM MEK
Boot: SD1
DRAM: 5.8 GiB
TCPC: Vendor ID [0x1fc9], Product ID [0x5110], Addr [I2C0 0x51]
MMC: FSL_SDHC: 0, FSL_SDHC: 1
Loading Environment from MMC... Run CMD11 1.8V switch
*** Warning - bad CRC, using default environment

 

We built a yocto build and SDK to build a surround view application.

However, we encountered the following error, and we are unable to proceed next because we cannot drive the camera.

 

root@imx8qmmek:~/surround-view-3D_1.1_beta/Tools/CamCapture# ./capturing
Failed to open input device
Failed to open input device
/dev/video0 is no video capture device
v4l_capture_setup failed camera 0

 

Is it because the camera doesn't recognize it? Or do we need another patch?

Our components used only genuine products from NXP.

 

regards!! and happy new year.

 

 

0 Kudos
Reply
1 Solution
3,060 Views
b36401
NXP Employee
NXP Employee

Possibly your OS (the image you built) can not recognize your camera.
Please make sure you are getting right device tree.

View solution in original post

0 Kudos
Reply
6 Replies
2,437 Views
diwakar2599
Contributor II

the same problem i'm facing and please tell me how to reslove this ?

0 Kudos
Reply
3,061 Views
b36401
NXP Employee
NXP Employee

Possibly your OS (the image you built) can not recognize your camera.
Please make sure you are getting right device tree.

0 Kudos
Reply
2,905 Views
kangmw086
Contributor III

I want to use three cameras to see the front screen like a panorama.

Is there a way?

 

regards!

0 Kudos
Reply
3,003 Views
kangmw086
Contributor III

hi

This problem has been solved.

One OV camera failed and the entire camera was not recognized.

0 Kudos
Reply
2,917 Views
songhongliang
Contributor II

HI,

Did you use surround-view-3D_1.1_beta to get surround view images?

0 Kudos
Reply
2,907 Views
kangmw086
Contributor III

yes.

360 degree screens are output.

0 Kudos
Reply