imx8qm surround view question.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

imx8qm surround view question.

跳至解决方案
3,285 次查看
kangmw086
Contributor III

I referred to the following documents of NXP.

(Surround View Application, User’s Guide, Rev. 1, 07/2018)

I purchased and installed all the components of the document.

i.mx8qm mek board u-boot message.

U-Boot 2018.03-4.14.98-2.3.3+gc20c44482b (Jan 10 2022 - 08:39:51 +0000)

CPU: Freescale i.MX8QM revB A53 at 1200 MHz at 32C
Model: Freescale i.MX8QM MEK
Board: iMX8QM MEK
Boot: SD1
DRAM: 5.8 GiB
TCPC: Vendor ID [0x1fc9], Product ID [0x5110], Addr [I2C0 0x51]
MMC: FSL_SDHC: 0, FSL_SDHC: 1
Loading Environment from MMC... Run CMD11 1.8V switch
*** Warning - bad CRC, using default environment

 

We built a yocto build and SDK to build a surround view application.

However, we encountered the following error, and we are unable to proceed next because we cannot drive the camera.

 

root@imx8qmmek:~/surround-view-3D_1.1_beta/Tools/CamCapture# ./capturing
Failed to open input device
Failed to open input device
/dev/video0 is no video capture device
v4l_capture_setup failed camera 0

 

Is it because the camera doesn't recognize it? Or do we need another patch?

Our components used only genuine products from NXP.

 

regards!! and happy new year.

 

 

0 项奖励
回复
1 解答
3,266 次查看
b36401
NXP Employee
NXP Employee

Possibly your OS (the image you built) can not recognize your camera.
Please make sure you are getting right device tree.

在原帖中查看解决方案

0 项奖励
回复
6 回复数
2,643 次查看
diwakar2599
Contributor II

the same problem i'm facing and please tell me how to reslove this ?

0 项奖励
回复
3,267 次查看
b36401
NXP Employee
NXP Employee

Possibly your OS (the image you built) can not recognize your camera.
Please make sure you are getting right device tree.

0 项奖励
回复
3,111 次查看
kangmw086
Contributor III

I want to use three cameras to see the front screen like a panorama.

Is there a way?

 

regards!

0 项奖励
回复
3,209 次查看
kangmw086
Contributor III

hi

This problem has been solved.

One OV camera failed and the entire camera was not recognized.

0 项奖励
回复
3,123 次查看
songhongliang
Contributor II

HI,

Did you use surround-view-3D_1.1_beta to get surround view images?

0 项奖励
回复
3,113 次查看
kangmw086
Contributor III

yes.

360 degree screens are output.

0 项奖励
回复