imx8qm mek lpuart0 init

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx8qm mek lpuart0 init

583 Views
rkohli2000
Contributor III

Hi, 

I'm building a custom app and need to init lpuart0, configure it (enable tx, set baud rate, etc) for basic output to the debug console (j18) without any u-boot or RTOS running. Is there any simple init example I can use that is not using CMSIS ?  Thanks.

0 Kudos
1 Reply

519 Views
igorpadykov
NXP Employee
NXP Employee

Hi rkohli2000

for lpuart examples one can look at SDK_MEK-MIMX8QM

available on https://community.nxp.com/community/mcuxpresso 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos