Hi guy,
I have searched NXP community, but I could find some of information on my issue,
As i mention on the subject, i have a problem to run MINISASTOCSI(mipi-ov5640) in imx8qm-mek.
To run mipi-ov5640, in uboot, I set up "setenv fdt_file fsl-imx8qm-mek-ov5640.dtb
below is error some of dmesg:
ov5640_mipi_v3 9-003c: 9-003c supplay DOVDD not found, using dummy regulator
ov5640_mipi_v3 9-003c: 9-003c suplpay DVDD not found, using dummy regulator
ov5640_mipi_v3 9-003c: 9-003c supplay AVDD not found, using dummy regulator
ov5640_mipi_v3 9-003c: Read reg error: reg=300a
It seems to be more setting up for running MINISASTOCSI, but i have no idea.
Could you tell me clues or link to refer?
I have one more question, there is no ov5640_mipi_v3 c file in git source. where can i find it?
Solved! Go to Solution.
I connected J10 port, how about using the commad:
gst-launch-1.0 v4l2src ! video/x-raw,width=640,height=480 ! waylandsink??
I have tested ov5640 on imx8qm successfully with 5.4.24 demo images, I used "imx8qm-mek-ov5640.dtb", when the board boot up, try to use the command like:
gst-launch-1.0 v4l2src ! video/x-raw,width=640,height=480 ! waylandsink
I checked the log file, I don't have ov5640_mipi_v3, and for source code, only have ov5640_mipi_v2
Hi guys,
I had tested 4.14.98 image and mipi_v3 log is from 4.14.98.
and I have tested new image is 5.4.47 and below dmesg :
NXP i.MX Release Distro 5.4-zeus imx8qmmek ttyLP0
imx8qmmek login: root
Last login: Thu Aug 20 05:03:54 UTC 2020 on tty7
root@imx8qmmek:~# demsg | grep ov5640
-sh: demsg: command not found
root@imx8qmmek:~# dmesg | grep ov5640
[ 2.896798] ov5640 5-003c: 5-003c supply DOVDD not found, using dummy regular
[ 2.904164] ov5640 5-003c: 5-003c supply AVDD not found, using dummy regulatr
[ 2.911425] ov5640 5-003c: 5-003c supply DVDD not found, using dummy regulatr
[ 2.966006] ov5640 5-003c: ov5640_read_reg: error: reg=300a
[ 2.971614] ov5640 5-003c: ov5640_check_chip_id: failed to read chip identifr
[ 2.979100] ov5640: probe of 5-003c failed with error -5
[ 2.990952] ov5640 6-003c: 6-003c supply DOVDD not found, using dummy regular
[ 2.998323] ov5640 6-003c: 6-003c supply AVDD not found, using dummy regulatr
[ 3.005604] ov5640 6-003c: 6-003c supply DVDD not found, using dummy regulatr
[ 3.060653] ov5640 6-003c: ov5640_read_reg: error: reg=300a
[ 3.066256] ov5640 6-003c: ov5640_check_chip_id: failed to read chip identifr
[ 3.073737] ov5640: probe of 6-003c failed with error -5
I have connected MINISASTOCSI to MIPI CSI0 or CSI1.
I connected J10 port, how about using the commad:
gst-launch-1.0 v4l2src ! video/x-raw,width=640,height=480 ! waylandsink??
Hi guys,
I have checked camera capture in 4.14.98-2.0.0
and gstreamer command is below:
gst-launch-1.0 v4l2src device=/dev/video0 ! video/x-raw,width=640,height=480 ! waylandsink
I unplugged SAS cable and plug in and remove tape on camera lens, and then retried.
Thank you for your comment about gstreamer cmds.