imx8qm m4 lvds1

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx8qm m4 lvds1

1,550 Views
337389696
Contributor I

Hello, is there any demo of imx8qm M4 using lvds1 dual channel?

pastedImage_1.png

Tags (1)
0 Kudos
Reply
2 Replies

1,385 Views
igorpadykov
NXP Employee
NXP Employee

Hi 军军 李 

one can check driver_examples../dpu/..display_interface.c
in M4 SDK MEK-MIMX8QM available on Welcome | MCUXpresso SDK Builder 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,384 Views
337389696
Contributor I

Thank you for your reply,

I looked at display_interface.c, but only channel 0 was used, I mean using both channel 0 and channel 1 of lvds1

Is there a use case for using 2 channels simultaneously

0 Kudos
Reply