imx8qm jailhouse

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

imx8qm jailhouse

1,603 次查看
Ahelion
Contributor IV

Hi all,

Is there any document showing all the steps to have a demo running on imx8qm mek board with jailhouse?

I was going over this: L5.4.70_2.3.3_LINUX_DOCS

but all I could find is a reference to device trees:

Hypervisor Jailhouse Enables the Jailhouse Hypervisor device trees.
• imx8qxp-mek-root.dtb: DTB for root-cell

I do not know what to do with this info. That is why I need a step by step instruction list.

Br, Mircea

 

标记 (1)
0 项奖励
回复
7 回复数

1,583 次查看
Rita_Wang
NXP TechSupport
NXP TechSupport

Which version BSP are you want to use?

0 项奖励
回复

1,579 次查看
Ahelion
Contributor IV

L5.4.70_2.3.3, i was following this quide, so all bsp-s mentioned here I am using.

0 项奖励
回复

1,576 次查看
Rita_Wang
NXP TechSupport
NXP TechSupport

OK, I will help confirm.

0 项奖励
回复

1,492 次查看
Ahelion
Contributor IV

any ideea? 

Found out that the latest linux kernel does support the lates XEN

How can I get Linux and Android running at the same time?

 

0 项奖励
回复

1,474 次查看
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi,

Yes, the xen is supported on the i.MX8QM.

You can refer to the attach document.

Wish you have a nice day

Best Regards

Rita

0 项奖励
回复

1,468 次查看
Ahelion
Contributor IV
I can tell you right now, it is not supported. I could not get jailhouse or xen to work on imx8qm. Whatever documentation i find is referencing linux4.9, which can not be build anymore.
0 项奖励
回复

972 次查看
Jerry137207
Contributor I

Hi, Ahelion:

I'm interested in runing multiple OS based on jailhouse, but related information is lack. I've sucessfully run jailhouse test demo in Imx8qm mek board. If you would like share info each other, plz email me: 1372071341@qq.com.

0 项奖励
回复