imx8qm hardware isolated using a72_0 to start second system kernel bug

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx8qm hardware isolated using a72_0 to start second system kernel bug

907件の閲覧回数
zbm030823
Contributor II

imx8qm hardware isolated using a72_0  to start second system kernel bug,could anyone help me?

Starting kernel ...

[    0.000000] Booting Linux on physical CPU 0x100

[    0.000000] Linux version 4.14.98+g1175b59 (root@adan-Standard-PC-i440FX-PIIX-1996) (gcc version 7.3.0 (GCC)) #19 SMP PREEMPT Tue Aug 27 17:39:15 CST 2019

[    0.000000] Boot CPU: AArch64 Processor [410fd082]

[    0.000000] a72boot_command_line = (�:


[    0.000000] Machine model: Freescale i.MX8QM MEK

[    0.000000] earlycon: lpuart32 at MMIO 0x000000005a060000 (options '115200')

[    0.000000] bootconsole [lpuart32] enabled

[    0.000000] a72 parse_early_param


[    0.000000] Bad mode in Error handler detected on CPU0, code 0xbf000002 -- SError

[    0.000000] Internal error: Oops - bad mode: 0 [#1] PREEMPT SMP

[    0.000000] Modules linked in:

[    0.000000] CPU: 0 PID: 0 Comm: swapper Not tainted 4.14.98+g1175b59 #19

[    0.000000] Hardware name: Freescale i.MX8QM MEK (DT)

[    0.000000] task: ffff000009452580 task.stack: ffff000009440000

[    0.000000] PC is at setup_arch+0x120/0x530

[    0.000000] LR is at setup_arch+0x11c/0x530

[    0.000000] pc : [<ffff0000093028c4>] lr : [<ffff0000093028c0>] pstate: 600000c5

[    0.000000] sp : ffff000009443f30

[    0.000000] x29: ffff000009443f30 x28: 00000000c1500018

[    0.000000] x27: 0000000000000400 x26: 00000000ffe79b90

[    0.000000] x25: 0000000000000000 x24: 00000000ffefb620

[    0.000000] x23: 0000000000000000 x22: ffff000009448000

[    0.000000] x21: ffff7dfffe8000c4 x20: ffff00000946a000

[    0.000000] x19: ffff000008080000 x18: 0000000000000010

[    0.000000] x17: 0000000000001800 x16: 0000000000000000

[    0.000000] x15: ffffffffffffffff x14: ffff0000895f4547

[    0.000000] x13: ffff0000095f4555 x12: ffff000009448df8

[    0.000000] x11: ffff000008632588 x10: ffff000009443c50

[    0.000000] x9 : 000000000000000d x8 : ffff000009443c20

[    0.000000] x7 : 0000000000000000 x6 : 0000000000000008

[    0.000000] x5 : 0000000000000000 x4 : 0000000000000000

[    0.000000] x3 : ffffffffffffffff x2 : ffff000009462f68

[    0.000000] x1 : ffff000009452580 x0 : 0000000000000016

[    0.000000] Process swapper (pid: 0, stack limit = 0xffff000009440000)

[    0.000000] Call trace:

[    0.000000] Exception stack(0xffff000009443df0 to 0xffff000009443f30)

[    0.000000] 3de0:                                   0000000000000016 ffff000009452580

[    0.000000] 3e00: ffff000009462f68 ffffffffffffffff 0000000000000000 0000000000000000

[    0.000000] 3e20: 0000000000000008 0000000000000000 ffff000009443c20 000000000000000d

[    0.000000] 3e40: ffff000009443c50 ffff000008632588 ffff000009448df8 ffff0000095f4555

[    0.000000] 3e60: ffff0000895f4547 ffffffffffffffff 0000000000000000 0000000000001800

[    0.000000] 3e80: 0000000000000010 ffff000008080000 ffff00000946a000 ffff7dfffe8000c4

[    0.000000] 3ea0: ffff000009448000 0000000000000000 00000000ffefb620 0000000000000000

[    0.000000] 3ec0: 00000000ffe79b90 0000000000000400 00000000c1500018 ffff000009443f30

[    0.000000] 3ee0: ffff0000093028c0 ffff000009443f30 ffff0000093028c4 00000000600000c5

[    0.000000] 3f00: 0000000000000072 0000000000000063 ffffffffffffffff 8080808080808000

[    0.000000] 3f20: ffff000009443f30 ffff0000093028c4

[    0.000000] [<ffff0000093028c4>] setup_arch+0x120/0x530

[    0.000000] [<ffff00000930083c>] start_kernel+0x64/0x3ac

[    0.000000] Code: f0fff240 91056000 97b85e23 d50344ff (b0fffc56)

[    0.000000] random: get_random_bytes called from print_oops_end_marker+0x4c/0x68 with crng_init=0

[    0.000000] ---[ end trace 0000000000000000 ]---

[    0.000000] Kernel panic - not syncing: Attempted to kill the idle task!

[    0.000000] ---[ end Kernel panic - not syncing: Attempted to kill the idle task!

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

819件の閲覧回数
CarlosCasillas
NXP Employee
NXP Employee

Hi,

I’m afraid that i.MX8QM family is still on preproduction and no additional information/support could be provided yet. For further assistance, please contact with your Sales/FAE.

Hope this will be useful for you.
Best regards!
/Carlos
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
-------------------------------------------------------------------------------

0 件の賞賛
返信

819件の閲覧回数
wuguangnan110
Contributor I

tell me please why the hardware isolated is not support for me ? sonofbitch

0 件の賞賛
返信

819件の閲覧回数
winters_chen
Contributor I

Hi ! wuguangnan110

I also met the same issue.I could not  use a72_0  to start second system kernel

Do you solve the problem?Could you please share the solution with us?

Appreciate your help!

Thank you !

0 件の賞賛
返信