imx8qm通过xen产生eth1不能通信

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx8qm通过xen产生eth1不能通信

2,041 Views
957992093
Contributor III

您好:

   使用android-p9_0_0-2_1_0过程中,通过xen启动配置网桥连接,产生eth0 和 eth1双网卡,eth1不能ping通网桥,已经配置成相同的网段,提示错误为connect: Network is unreachable,eth0能正常通信。之前在android上添加usb网卡,网卡名是usb0,配置好ip,网关,路由,dns也是不能联网,后来把usb0网卡名修改成eth0网卡可以正常使用,请问android程序里对eth0做什么特别操作了么?还有需要配置什么才可以让android在除eth0网卡名外的网卡上网,比如usb0,像这种驱动都正常,配置也没问题,为什么提示connect: Network is unreachable?

0 Kudos
Reply
1 Reply

1,836 Views
myy
Contributor II
请问如何配置xen产生eth1和eth0
0 Kudos
Reply