imx8plus npu per-tensor vs per-channel

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

imx8plus npu per-tensor vs per-channel

214 次查看
dk93
Contributor I

i have a custom trained keras model, mobilenetv1 and having the imx8plus evk targeting its NPU.

i have done PTQ and QAT quantizations to tflite int8, with: 

converter._experimental_disable_per_channel = True

PTQ i get 3.5ms inference, just as benchmarks on imx8p npu has shown. and i understand that PTQ does use per-tensor quant so it is fast as the NXP benchmarks, but it does have an accuracy loss vs original.

my qat model, which shows superior accuracy vs PTQ, seems to be 2x slower, at 7ms inference. 

My understanding is that TF-QAT by default uses per-channel quantization.
My question is is there a way to enable per-tensor for QAT? either before fine-tuning or during tflite conversion?

标记 (1)
0 项奖励
回复
0 回复数