imx8mqevk, copying rootfs to SD card

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

imx8mqevk, copying rootfs to SD card

1,861 次查看
jekim
Contributor IV

Linux : Ubuntu 16.04

I've already copied bootloader(flash.bin) into the 1st partition of SD card.

I'm trying to copy rootfs into the 2nd partition according Linux User Guide. I quote the instruction below.

"Extract a rootfs package to a directory: for example, extract fsl-image-qt5-validation-imx-imx7ulpevk.tar.bz2
to /home/user/rootfs for example:"

Btw, how to extract the bz2 file from where?

My board is imx8mqevk. Is the bz2 file above compatible with my board?

标签 (1)
标记 (1)
0 项奖励
回复
3 回复数

1,558 次查看
Rita_Wang
NXP TechSupport
NXP TechSupport

Which version BSP are you using?

0 项奖励
回复

1,558 次查看
jekim
Contributor IV

Hi Rita,

Extracting the ba2 file can be done by "bitbake fsl-image-validation-imx DISTRO=fsl-imx-wayland MACHINE=imx8mqevk" as far as tried for example.

As a result of bitbake command, I've got fsl-image-validation-imx-imx8mqevk.tar.bz2 file under build_wayland/tmp/work/.... /deploy-fsl-image-validation-imx-image-complete folder. If you know better way, please let me know.

Regards,

Jeff

0 项奖励
回复

1,557 次查看
jekim
Contributor IV

imx-yocto-L4.9.88_2.0.0

0 项奖励
回复