imx8mq yocto zeus err.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx8mq yocto zeus err.

ソリューションへジャンプ
5,181件の閲覧回数
kangmw086
Contributor III

hi

i used imx8mq-evk.

yocto[zeus] kernel version. 5.4.70_2.3.0

I completed the YOCTO build and fused it into SD Card before running it.

I think the following error occurred, but I don't know how to solve it. Can you help me?

 

U-Boot SPL 2020.04-5.4.70-2.3.0+ge42dee8 (Jan 27 2021 - 08:29:45 +0000)
PMIC: PFUZE100 ID=0x10
DDRINFO: start DRAM init
DDRINFO: DRAM rate 3200MTS
DDRINFO:ddrphy calibration done
DDRINFO: ddrmix config done
Normal Boot
Trying to boot from MMC2
E/TC:0 0 caam_mp_init:364 *************************************
E/TC:0 0 caam_mp_init:365 * Warning: Manufacturing protection *
E/TC:0 0 caam_mp_init:366 * is not supported *
E/TC:0 0 caam_mp_init:367 *************************************


U-Boot 2020.04-5.4.70-2.3.0+ge42dee8 (Jan 27 2021 - 08:29:45 +0000)

CPU: i.MX8MQ rev2.0 1500 MHz (running at 1000 MHz)
CPU: Commercial temperature grade (0C to 95C) at 57C
Reset cause: POR
Model: NXP i.MX8MQ EVK
DRAM: 3 GiB
TCPC: Vendor ID [0x1fc9], Product ID [0x5110], Addr [I2C0 0x50]
MMC: FSL_SDHC: 0, FSL_SDHC: 1
Loading Environment from MMC... Run CMD11 1.8V switch
*** Warning - bad CRC, using default environment

[*]-Video Link 0imx8m_hdmi_probe
(1280 x 720)
[0] display-controller@32e00000, video
[1] hdmi@32c00000, display
In: serial
Out: serial
Err: serial

BuildInfo:
- ATF f1d7187
- U-Boot 2020.04-5.4.70-2.3.0+ge42dee8

Run CMD11 1.8V switch
switch to partitions #0, OK
mmc1 is current device
flash target is MMC:1
Run CMD11 1.8V switch
Net:
Error: ethernet@30be0000 address not set.

Error: ethernet@30be0000 address not set.
No ethernet found.

Fastboot: Normal
Normal Boot
Hit any key to stop autoboot: 0
Run CMD11 1.8V switch
switch to partitions #0, OK
mmc1 is current device
Run CMD11 1.8V switch
28013056 bytes read in 449 ms (59.5 MiB/s)
Booting from mmc ...
45027 bytes read in 23 ms (1.9 MiB/s)
## Flattened Device Tree blob at 43000000
Booting using the fdt blob at 0x43000000
Using Device Tree in place at 0000000043000000, end 000000004300dfe2

Starting kernel ...

[ 0.000000] Booting Linux on physical CPU 0x0000000000 [0x410fd034]
[ 0.000000] Linux version 5.4.70-2.3.0+g4f2631b (oe-user@oe-host) (gcc version 9.2.0 (GCC)) #1 SMP PREEMPT Thu Jan 28 05
:36:23 UTC 2021
[ 0.000000] Machine model: NXP i.MX8MQ EVK
[ 0.000000] efi: Getting EFI parameters from FDT:
[ 0.000000] efi: UEFI not found.
[ 0.000000] Reserved memory: created CMA memory pool at 0x0000000044000000, size 960 MiB
[ 0.000000] OF: reserved mem: initialized node linux,cma, compatible id shared-dma-pool
[ 0.000000] NUMA: No NUMA configuration found
[ 0.000000] NUMA: Faking a node at [mem 0x0000000040000000-0x00000000fdffffff]
[ 0.000000] NUMA: NODE_DATA [mem 0xfd9de500-0xfd9dffff]
[ 0.000000] Zone ranges:
[ 0.000000] DMA32 [mem 0x0000000040000000-0x00000000fdffffff]
[ 0.000000] Normal empty
[ 0.000000] Movable zone start for each node
[ 0.000000] Early memory node ranges
[ 0.000000] node 0: [mem 0x0000000040000000-0x00000000b7ffffff]
[ 0.000000] node 0: [mem 0x00000000b8400000-0x00000000fdffffff]
[ 0.000000] Initmem setup node 0 [mem 0x0000000040000000-0x00000000fdffffff]
[ 0.000000] psci: probing for conduit method from DT.
[ 0.000000] psci: PSCIv1.1 detected in firmware.
[ 0.000000] psci: Using standard PSCI v0.2 function IDs
[ 0.000000] psci: Trusted OS migration not required
[ 0.000000] psci: SMC Calling Convention v1.1
[ 0.000000] percpu: Embedded 24 pages/cpu s58904 r8192 d31208 u98304
[ 0.000000] Detected VIPT I-cache on CPU0
[ 0.000000] CPU features: detected: ARM erratum 845719
[ 0.000000] CPU features: detected: GIC system register CPU interface
[ 0.000000] Speculative Store Bypass Disable mitigation not required
[ 0.000000] Built 1 zonelists, mobility grouping on. Total pages: 765056
[ 0.000000] Policy zone: DMA32
[ 0.000000] Kernel command line: console=ttymxc0,115200 root=/dev/mmcblk1p2 rootwait rw
[ 0.000000] Dentry cache hash table entries: 524288 (order: 10, 4194304 bytes, linear)
[ 0.000000] Inode-cache hash table entries: 262144 (order: 9, 2097152 bytes, linear)
[ 0.000000] mem auto-init: stack:off, heap alloc:off, heap free:off
[ 0.000000] Memory: 2035416K/3108864K available (16636K kernel code, 1244K rwdata, 6556K rodata, 2880K init, 1017K bss,
90408K reserved, 983040K cma-reserved)
[ 0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=4, Nodes=1
[ 0.000000] rcu: Preemptible hierarchical RCU implementation.
[ 0.000000] rcu: RCU restricting CPUs from NR_CPUS=256 to nr_cpu_ids=4.
[ 0.000000] Tasks RCU enabled.
[ 0.000000] rcu: RCU calculated value of scheduler-enlistment delay is 25 jiffies.
[ 0.000000] rcu: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=4
[ 0.000000] NR_IRQS: 64, nr_irqs: 64, preallocated irqs: 0
[ 0.000000] GICv3: GIC: Using split EOI/Deactivate mode
[ 0.000000] GICv3: 128 SPIs implemented
[ 0.000000] GICv3: 0 Extended SPIs implemented
[ 0.000000] GICv3: Distributor has no Range Selector support
[ 0.000000] GICv3: 16 PPIs implemented
[ 0.000000] GICv3: no VLPI support, no direct LPI support
[ 0.000000] GICv3: CPU0: found redistributor 0 region 0:0x0000000038880000
[ 0.000000] ITS: No ITS available, not enabling LPIs
[ 0.000000] random: get_random_bytes called from start_kernel+0x2b8/0x44c with crng_init=0
[ 0.000000] arch_timer: cp15 timer(s) running at 8.33MHz (phys).
[ 0.000000] clocksource: arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x1ec0311ec, max_idle_ns: 440795202152 ns
[ 0.000004] sched_clock: 56 bits at 8MHz, resolution 120ns, wraps every 2199023255541ns
[ 0.000489] Console: colour dummy device 80x25
[ 0.000562] Calibrating delay loop (skipped), value calculated using timer frequency.. 16.66 BogoMIPS (lpj=33333)
[ 0.000573] pid_max: default: 32768 minimum: 301
[ 0.000658] LSM: Security Framework initializing
[ 0.000728] Mount-cache hash table entries: 8192 (order: 4, 65536 bytes, linear)
[ 0.000751] Mountpoint-cache hash table entries: 8192 (order: 4, 65536 bytes, linear)
[ 0.002075] ASID allocator initialised with 32768 entries
[ 0.002156] rcu: Hierarchical SRCU implementation.
[ 0.003208] EFI services will not be available.
[ 0.003394] smp: Bringing up secondary CPUs ...
[ 0.003822] Detected VIPT I-cache on CPU1
[ 0.003847] GICv3: CPU1: found redistributor 1 region 0:0x00000000388a0000
[ 0.003871] CPU1: Booted secondary processor 0x0000000001 [0x410fd034]
[ 0.004361] Detected VIPT I-cache on CPU2
[ 0.004379] GICv3: CPU2: found redistributor 2 region 0:0x00000000388c0000
[ 0.004396] CPU2: Booted secondary processor 0x0000000002 [0x410fd034]
[ 0.004824] Detected VIPT I-cache on CPU3
[ 0.004842] GICv3: CPU3: found redistributor 3 region 0:0x00000000388e0000
[ 0.004859] CPU3: Booted secondary processor 0x0000000003 [0x410fd034]
[ 0.004928] smp: Brought up 1 node, 4 CPUs
[ 0.004946] SMP: Total of 4 processors activated.
[ 0.004955] CPU features: detected: 32-bit EL0 Support
[ 0.004963] CPU features: detected: CRC32 instructions
[ 0.013554] CPU: All CPU(s) started at EL2
[ 0.013580] alternatives: patching kernel code
[ 0.015195] devtmpfs: initialized
[ 0.022456] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 7645041785100000 ns
[ 0.022474] futex hash table entries: 1024 (order: 4, 65536 bytes, linear)
[ 0.051280] pinctrl core: initialized pinctrl subsystem
[ 0.052146] DMI not present or invalid.
[ 0.052428] NET: Registered protocol family 16
[ 0.059903] DMA: preallocated 256 KiB pool for atomic allocations
[ 0.059919] audit: initializing netlink subsys (disabled)
[ 0.060075] audit: type=2000 audit(0.056:1): state=initialized audit_enabled=0 res=1
[ 0.061034] cpuidle: using governor menu
[ 0.061540] hw-breakpoint: found 6 breakpoint and 4 watchpoint registers.
[ 0.062493] Serial: AMBA PL011 UART driver
[ 0.062565] imx mu driver is registered.
[ 0.062590] imx rpmsg driver is registered.
[ 0.066577] imx8mq-pinctrl 30330000.iomuxc: initialized IMX pinctrl driver
[ 0.092370] HugeTLB registered 1.00 GiB page size, pre-allocated 0 pages
[ 0.092380] HugeTLB registered 32.0 MiB page size, pre-allocated 0 pages
[ 0.092389] HugeTLB registered 2.00 MiB page size, pre-allocated 0 pages
[ 0.092397] HugeTLB registered 64.0 KiB page size, pre-allocated 0 pages
[ 0.093400] cryptd: max_cpu_qlen set to 1000
[ 0.096873] ACPI: Interpreter disabled.
[ 0.097770] iommu: Default domain type: Translated
[ 0.097932] vgaarb: loaded
[ 0.098253] SCSI subsystem initialized
[ 0.098662] usbcore: registered new interface driver usbfs
[ 0.098709] usbcore: registered new interface driver hub
[ 0.098781] usbcore: registered new device driver usb
[ 0.099843] mc: Linux media interface: v0.10
[ 0.099874] videodev: Linux video capture interface: v2.00
[ 0.099944] pps_core: LinuxPPS API ver. 1 registered
[ 0.099951] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
[ 0.099967] PTP clock support registered
[ 0.100102] EDAC MC: Ver: 3.0.0
[ 0.100903] No BMan portals available!
[ 0.101203] QMan: Allocated lookup table at (____ptrval____), entry count 65537
[ 0.101530] No QMan portals available!
[ 0.102010] No USDPAA memory, no 'fsl,usdpaa-mem' in device-tree
[ 0.102400] FPGA manager framework
[ 0.102498] Advanced Linux Sound Architecture Driver Initialized.
[ 0.102920] Bluetooth: Core ver 2.22
[ 0.102946] NET: Registered protocol family 31
[ 0.102951] Bluetooth: HCI device and connection manager initialized
[ 0.102966] Bluetooth: HCI socket layer initialized
[ 0.102974] Bluetooth: L2CAP socket layer initialized
[ 0.102990] Bluetooth: SCO socket layer initialized
[ 0.103650] clocksource: Switched to clocksource arch_sys_counter
[ 0.103810] VFS: Disk quotas dquot_6.6.0
[ 0.103863] VFS: Dquot-cache hash table entries: 512 (order 0, 4096 bytes)
[ 0.104030] pnp: PnP ACPI: disabled
[ 0.110531] thermal_sys: Registered thermal governor 'step_wise'
[ 0.110535] thermal_sys: Registered thermal governor 'power_allocator'
[ 0.110837] NET: Registered protocol family 2
[ 0.111177] tcp_listen_portaddr_hash hash table entries: 2048 (order: 3, 32768 bytes, linear)
[ 0.111234] TCP established hash table entries: 32768 (order: 6, 262144 bytes, linear)
[ 0.111484] TCP bind hash table entries: 32768 (order: 7, 524288 bytes, linear)
[ 0.112031] TCP: Hash tables configured (established 32768 bind 32768)
[ 0.112124] UDP hash table entries: 2048 (order: 4, 65536 bytes, linear)
[ 0.112213] UDP-Lite hash table entries: 2048 (order: 4, 65536 bytes, linear)
[ 0.112402] NET: Registered protocol family 1
[ 0.112749] RPC: Registered named UNIX socket transport module.
[ 0.112755] RPC: Registered udp transport module.
[ 0.112761] RPC: Registered tcp transport module.
[ 0.112766] RPC: Registered tcp NFSv4.1 backchannel transport module.
[ 0.113143] PCI: CLS 0 bytes, default 64
[ 0.113846] hw perfevents: enabled with armv8_cortex_a53 PMU driver, 7 counters available
[ 0.114201] kvm [1]: IPA Size Limit: 40bits
[ 0.115382] kvm [1]: vgic-v2@31020000
[ 0.115403] kvm [1]: GIC system register CPU interface enabled
[ 0.115467] kvm [1]: vgic interrupt IRQ1
[ 0.115585] kvm [1]: Hyp mode initialized successfully
[ 0.118673] Initialise system trusted keyrings
[ 0.118773] workingset: timestamp_bits=44 max_order=20 bucket_order=0
[ 0.125681] squashfs: version 4.0 (2009/01/31) Phillip Lougher
[ 0.126353] NFS: Registering the id_resolver key type
[ 0.126378] Key type id_resolver registered
[ 0.126383] Key type id_legacy registered
[ 0.126410] nfs4filelayout_init: NFSv4 File Layout Driver Registering...
[ 0.126432] jffs2: version 2.2. (NAND) �© 2001-2006 Red Hat, Inc.
[ 0.126818] 9p: Installing v9fs 9p2000 file system support
[ 0.142848] Key type asymmetric registered
[ 0.142855] Asymmetric key parser 'x509' registered
[ 0.142887] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 244)
[ 0.142894] io scheduler mq-deadline registered
[ 0.142899] io scheduler kyber registered
[ 0.148268] EINJ: ACPI disabled.
[ 0.156665] imx-sdma 302c0000.dma-controller: Direct firmware load for imx/sdma/sdma-imx7d.bin failed with error -2
[ 0.156677] imx-sdma 302c0000.dma-controller: Falling back to sysfs fallback for: imx/sdma/sdma-imx7d.bin
[ 0.161815] mxs-dma 33000000.dma-apbh: initialized
[ 0.165552] Bus freq driver module loaded
[ 0.165778] Config NOC for VPU and CPU
[ 0.170146] Serial: 8250/16550 driver, 4 ports, IRQ sharing enabled
[ 0.172197] 30860000.serial: ttymxc0 at MMIO 0x30860000 (irq = 31, base_baud = 1562500) is a IMX
[ 1.136323] printk: console [ttymxc0] enabled
[ 1.141150] 30890000.serial: ttymxc1 at MMIO 0x30890000 (irq = 32, base_baud = 1562500) is a IMX
[ 1.158703] imx-dcss 32e00000.display-controller: ctxld: can't get irq number
[ 1.165920] imx-dcss 32e00000.display-controller: submodules initialization failed
[ 1.184064] loop: module loaded
[ 1.189394] imx ahci driver is registered.
[ 1.196255] spi-nor spi3.0: n25q256a (32768 Kbytes)
[ 1.206019] libphy: Fixed MDIO Bus: probed
[ 1.211027] tun: Universal TUN/TAP device driver, 1.6
[ 1.216789] thunder_xcv, ver 1.0
[ 1.220064] thunder_bgx, ver 1.0
[ 1.223330] nicpf, ver 1.0
[ 1.226764] pps pps0: new PPS source ptp0
[ 1.236311] Freescale FM module, FMD API version 21.1.0
[ 1.241815] Freescale FM Ports module
[ 1.245492] fsl_mac: fsl_mac: FSL FMan MAC API based driver
[ 1.251227] fsl_dpa: FSL DPAA Ethernet driver
[ 1.255718] fsl_advanced: FSL DPAA Advanced drivers:
[ 1.260697] fsl_proxy: FSL DPAA Proxy initialization driver
[ 1.266378] fsl_oh: FSL FMan Offline Parsing port driver
[ 1.272624] hclge is initializing
[ 1.275952] hns3: Hisilicon Ethernet Network Driver for Hip08 Family - version
[ 1.283182] hns3: Copyright (c) 2017 Huawei Corporation.
[ 1.288551] e1000: Intel(R) PRO/1000 Network Driver - version 7.3.21-k8-NAPI
[ 1.295606] e1000: Copyright (c) 1999-2006 Intel Corporation.
[ 1.301399] e1000e: Intel(R) PRO/1000 Network Driver - 3.2.6-k
[ 1.307239] e1000e: Copyright(c) 1999 - 2015 Intel Corporation.
[ 1.313209] igb: Intel(R) Gigabit Ethernet Network Driver - version 5.6.0-k
[ 1.320180] igb: Copyright (c) 2007-2014 Intel Corporation.
[ 1.325794] igbvf: Intel(R) Gigabit Virtual Function Network Driver - version 2.4.0-k
[ 1.333636] igbvf: Copyright (c) 2009 - 2012 Intel Corporation.
[ 1.339731] sky2: driver version 1.30
[ 1.344364] VFIO - User Level meta-driver version: 0.3
[ 1.351924] ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
[ 1.358469] ehci-pci: EHCI PCI platform driver
[ 1.362958] ehci-platform: EHCI generic platform driver
[ 1.368368] ohci_hcd: USB 1.1 'Open' Host Controller (OHCI) Driver
[ 1.374567] ohci-pci: OHCI PCI platform driver
[ 1.379053] ohci-platform: OHCI generic platform driver
[ 1.384969] usbcore: registered new interface driver uas
[ 1.390332] usbcore: registered new interface driver usb-storage
[ 1.396413] usbcore: registered new interface driver usbserial_generic
[ 1.402965] usbserial: USB Serial support registered for generic
[ 1.409012] usbcore: registered new interface driver ftdi_sio
[ 1.414786] usbserial: USB Serial support registered for FTDI USB Serial Device
[ 1.422131] usbcore: registered new interface driver usb_serial_simple
[ 1.428685] usbserial: USB Serial support registered for carelink
[ 1.434803] usbserial: USB Serial support registered for zio
[ 1.440491] usbserial: USB Serial support registered for funsoft
[ 1.446524] usbserial: USB Serial support registered for flashloader
[ 1.452903] usbserial: USB Serial support registered for google
[ 1.458847] usbserial: USB Serial support registered for libtransistor
[ 1.465404] usbserial: USB Serial support registered for vivopay
[ 1.471433] usbserial: USB Serial support registered for moto_modem
[ 1.477727] usbserial: USB Serial support registered for motorola_tetra
[ 1.484367] usbserial: USB Serial support registered for novatel_gps
[ 1.490744] usbserial: USB Serial support registered for hp4x
[ 1.496518] usbserial: USB Serial support registered for suunto
[ 1.502468] usbserial: USB Serial support registered for siemens_mpi
[ 1.508863] usbcore: registered new interface driver usb_ehset_test
[ 1.517801] input: 30370000.snvs:snvs-powerkey as /devices/platform/soc@0/soc@0:bus@30000000/30370000.snvs/30370000.snvs
:snvs-powerkey/input/input0
[ 1.532948] snvs_rtc 30370000.snvs:snvs-rtc-lp: registered as rtc0
[ 1.539232] i2c /dev entries driver
[ 1.543333] mx6s-csi 30a90000.csi1_bridge: initialising
[ 1.551157] imx2-wdt 30280000.watchdog: timeout 60 sec (nowayout=0)
[ 1.557726] Bluetooth: HCI UART driver ver 2.3
[ 1.562182] Bluetooth: HCI UART protocol H4 registered
[ 1.567332] Bluetooth: HCI UART protocol BCSP registered
[ 1.572675] Bluetooth: HCI UART protocol LL registered
[ 1.577823] Bluetooth: HCI UART protocol ATH3K registered
[ 1.583254] Bluetooth: HCI UART protocol Three-wire (H5) registered
[ 1.589615] Bluetooth: HCI UART protocol Broadcom registered
[ 1.595303] Bluetooth: HCI UART protocol QCA registered
[ 1.602819] sdhci: Secure Digital Host Controller Interface driver
[ 1.609009] sdhci: Copyright(c) Pierre Ossman
[ 1.613563] Synopsys Designware Multimedia Card Interface Driver
[ 1.620207] sdhci-pltfm: SDHCI platform and OF driver helper
[ 1.628408] ledtrig-cpu: registered to indicate activity on CPUs
[ 1.635591] caam 30900000.crypto: device ID = 0x0a16040100000000 (Era 9)
[ 1.642309] caam 30900000.crypto: job rings = 2, qi = 0
[ 1.663346] caam algorithms registered in /proc/crypto
[ 1.669415] caam 30900000.crypto: caam pkc algorithms registered in /proc/crypto
[ 1.676833] caam 30900000.crypto: registering rng-caam
[ 1.682734] Device caam-keygen registered
[ 1.688412] caam-snvs 30370000.caam-snvs: violation handlers armed - non-secure state
[ 1.696951] usbcore: registered new interface driver usbhid
[ 1.702537] usbhid: USB HID core driver
[ 1.708238] No fsl,qman node
[ 1.711121] Freescale USDPAA process driver
[ 1.715333] fsl-usdpaa: no region found
[ 1.719175] Freescale USDPAA process IRQ driver
[ 1.727359] optee: probing for conduit method from DT.
[ 1.732535] optee: revision 3.10 (a991c904)
[ 1.733805] optee: dynamic shared memory is enabled
[ 1.743259] optee: initialized driver
[ 1.744339] random: fast init done
[ 1.750916] wm8524-codec audio-codec: Failed to get mute line: -517
[ 1.765846] imx-spdif sound-spdif: ASoC: failed to init link S/PDIF PCM: -517
[ 1.769126] random: crng init done
[ 1.773046] imx-spdif sound-hdmi-arc: ASoC: failed to init link S/PDIF PCM: -517
[ 1.784368] imx-ak4458 sound-ak4458: failed to find SAI platform device
[ 1.791003] imx-ak4458: probe of sound-ak4458 failed with error -22
[ 1.797515] imx-ak5558 sound-ak5558: failed to find SAI platform device
[ 1.804150] imx-ak5558: probe of sound-ak5558 failed with error -22
[ 1.811049] imx-cdnhdmi sound-hdmi: ASoC: failed to init link imx8 hdmi: -517
[ 1.818203] imx-cdnhdmi sound-hdmi: snd_soc_register_card failed (-517)
[ 1.825193] pktgen: Packet Generator for packet performance testing. Version: 2.75
[ 1.842927] NET: Registered protocol family 26
[ 1.848054] NET: Registered protocol family 10
[ 1.853151] Segment Routing with IPv6
[ 1.856913] NET: Registered protocol family 17
[ 1.861955] Bluetooth: RFCOMM TTY layer initialized
[ 1.866851] Bluetooth: RFCOMM socket layer initialized
[ 1.872040] Bluetooth: RFCOMM ver 1.11
[ 1.875812] Bluetooth: BNEP (Ethernet Emulation) ver 1.3
[ 1.881147] Bluetooth: BNEP filters: protocol multicast
[ 1.886385] Bluetooth: BNEP socket layer initialized
[ 1.891358] Bluetooth: HIDP (Human Interface Emulation) ver 1.2
[ 1.897302] Bluetooth: HIDP socket layer initialized
[ 1.902310] 8021q: 802.1Q VLAN Support v1.8
[ 1.906528] lib80211: common routines for IEEE802.11 drivers
[ 1.912316] 9pnet: Installing 9P2000 support
[ 1.916627] tsn generic netlink module v1 init...
[ 1.921424] Key type dns_resolver registered
[ 1.927101] registered taskstats version 1
[ 1.931227] Loading compiled-in X.509 certificates
[ 1.962841] ov5640_mipi 0-003c: No sensor reset pin available
[ 1.968635] ov5640_mipi 0-003c: 0-003c supply DOVDD not found, using dummy regulator
[ 1.976440] ov5640_mipi 0-003c: 0-003c supply DVDD not found, using dummy regulator
[ 1.984143] ov5640_mipi 0-003c: 0-003c supply AVDD not found, using dummy regulator
[ 2.005016] ov5640_mipi 0-003c: Read reg error: reg=300a
[ 2.010347] ov5640_mipi 0-003c: Camera is not found
[ 2.016834] pfuze100-regulator 0-0008: Full layer: 2, Metal layer: 1
[ 2.023823] pfuze100-regulator 0-0008: FAB: 0, FIN: 0
[ 2.028903] pfuze100-regulator 0-0008: pfuze100 found.
[ 2.062317] i2c i2c-0: IMX I2C adapter registered
[ 2.068362] ov5640_mipi 1-003c: No sensor reset pin available
[ 2.074153] ov5640_mipi 1-003c: 1-003c supply DOVDD not found, using dummy regulator
[ 2.081963] ov5640_mipi 1-003c: 1-003c supply DVDD not found, using dummy regulator
[ 2.089673] ov5640_mipi 1-003c: 1-003c supply AVDD not found, using dummy regulator
[ 2.107955] ov5640_mipi 1-003c: Read reg error: reg=300a
[ 2.113285] ov5640_mipi 1-003c: Camera is not found
[ 2.118327] i2c i2c-1: IMX I2C adapter registered
[ 2.124341] ak4458 2-0010: 2-0010 supply DVDD not found, using dummy regulator
[ 2.131623] ak4458 2-0010: 2-0010 supply AVDD not found, using dummy regulator
[ 2.139766] ak4458 2-0012: 2-0012 supply DVDD not found, using dummy regulator
[ 2.147080] ak4458 2-0012: 2-0012 supply AVDD not found, using dummy regulator
[ 2.155213] ak5558 2-0013: 2-0013 supply DVDD not found, using dummy regulator
[ 2.162491] ak5558 2-0013: 2-0013 supply AVDD not found, using dummy regulator
[ 2.170592] ak4458 2-0011: 2-0011 supply DVDD not found, using dummy regulator
[ 2.177870] ak4458 2-0011: 2-0011 supply AVDD not found, using dummy regulator
[ 2.185735] i2c i2c-2: IMX I2C adapter registered
[ 2.190954] imx8mq-usb-phy 381f0040.usb-phy: 381f0040.usb-phy supply vbus not found, using dummy regulator
[ 2.200902] imx8mq-usb-phy 382f0040.usb-phy: 382f0040.usb-phy supply vbus not found, using dummy regulator
[ 2.217320] [drm] Supports vblank timestamp caching Rev 2 (21.10.2013).
[ 2.223952] [drm] No driver support for vblank timestamp query.
[ 2.232404] cdns-mhdp-imx 32c00000.hdmi: lane-mapping 0xe4
[ 2.242324] imx-dcss 32e00000.display-controller: bound 32c00000.hdmi (ops cdns_mhdp_imx_ops)
[ 2.252222] [drm] Initialized imx-dcss 1.0.0 20190917 for 32e00000.display-controller on minor 0
[ 2.288635] cdns-mhdp-imx 32c00000.hdmi: 0,ff,ff,ff,ff,ff,ff,0
[ 2.329025] cdns-mhdp-imx 32c00000.hdmi: 0,ff,ff,ff,ff,ff,ff,0
[ 2.329856] [drm] Mode: 1920x1080p148500
[ 2.355662] [drm] Pixel clock: 148500 KHz, character clock: 148500, bpc is 8-bit.
[ 2.355666] [drm] VCO frequency is 5940000 KHz
[ 2.469363] [drm] Sink Not Support SCDC
[ 2.470592] [drm] No vendor infoframe
[ 2.567286] Console: switching to colour frame buffer device 240x67
[ 2.634396] imx-dcss 32e00000.display-controller: fb0: imx-dcssdrmfb frame buffer device
[ 2.644774] pps pps0: new PPS source ptp0
[ 2.654599] fec 30be0000.ethernet: Invalid MAC address: 00:00:00:00:00:00
[ 2.661419] fec 30be0000.ethernet: Using random MAC address: 7a:a8:f7:ad:6f:de
[ 2.669747] libphy: fec_enet_mii_bus: probed
[ 2.678881] fec 30be0000.ethernet eth0: registered PHC device 0
[ 2.685802] OF: graph: no port node found in /soc@0/usb-phy@381f0040
[ 2.693208] xhci-hcd xhci-hcd.1.auto: xHCI Host Controller
[ 2.698722] xhci-hcd xhci-hcd.1.auto: new USB bus registered, assigned bus number 1
[ 2.706515] xhci-hcd xhci-hcd.1.auto: hcc params 0x0220fe6c hci version 0x110 quirks 0x0000000001010010
[ 2.715968] xhci-hcd xhci-hcd.1.auto: irq 51, io mem 0x38200000
[ 2.723624] hub 1-0:1.0: USB hub found
[ 2.727413] hub 1-0:1.0: 1 port detected
[ 2.731621] xhci-hcd xhci-hcd.1.auto: xHCI Host Controller
[ 2.737136] xhci-hcd xhci-hcd.1.auto: new USB bus registered, assigned bus number 2
[ 2.744828] xhci-hcd xhci-hcd.1.auto: Host supports USB 3.0 SuperSpeed
[ 2.751424] usb usb2: We don't know the algorithms for LPM for this host, disabling LPM.
[ 2.760494] hub 2-0:1.0: USB hub found
[ 2.764276] hub 2-0:1.0: 1 port detected
[ 2.769327] imx-cpufreq-dt imx-cpufreq-dt: cpu speed grade 3 mkt segment 0 supported-hw 0x8 0x1
[ 2.804575] mmc0: SDHCI controller on 30b40000.mmc [30b40000.mmc] using ADMA
[ 2.812632] sdhci-esdhc-imx 30b50000.mmc: Got CD GPIO
[ 2.849456] mmc1: SDHCI controller on 30b50000.mmc [30b50000.mmc] using ADMA
[ 2.859349] galcore: clk_get 2d core clock failed, disable 2d/vg!
[ 2.865785] Galcore version 6.4.3.p1.305572
[ 2.923095] mmc0: new HS400 MMC card at address 0001
[ 2.943854] mmcblk0: mmc0:0001 R1J56L 13.8 GiB
[ 2.948554] mmcblk0boot0: mmc0:0001 R1J56L partition 1 4.00 MiB
[ 2.967471] mmcblk0boot1: mmc0:0001 R1J56L partition 2 4.00 MiB
[ 2.974145] mmcblk0rpmb: mmc0:0001 R1J56L partition 3 128 KiB, chardev (237:0)
[ 3.005044] [drm] Initialized vivante 1.0.0 20170808 for 38000000.gpu3d on minor 1
[ 3.018328] hantrodec: module inserted. Major = 236
[ 3.026226] mmc1: host does not support reading read-only switch, assuming write-enable
[ 3.035961] debugfs: Directory '308b0000.sai' with parent 'wm8524-audio' already present!
[ 3.044243] asoc-simple-card sound-wm8524: wm8524-hifi <-> 308b0000.sai mapping ok
[ 3.051890] asoc-simple-card sound-wm8524: ASoC: no DMI vendor name!
[ 3.059971] imx-spdif sound-spdif: ASoC: failed to init link S/PDIF PCM: -517
[ 3.067574] imx-spdif sound-hdmi-arc: ASoC: failed to init link S/PDIF PCM: -517
[ 3.067660] usb 1-1: new high-speed USB device number 2 using xhci-hcd
[ 3.075586] debugfs: Directory '30050000.sai' with parent 'imx-audio-hdmi' already present!
[ 3.089979] imx-cdnhdmi sound-hdmi: i2s-hifi <-> 30050000.sai mapping ok
[ 3.096720] imx-cdnhdmi sound-hdmi: ASoC: no DMI vendor name!
[ 3.102524] debugfs: File 'Capture' in directory 'dapm' already present!
[ 3.110579] input: imx-audio-hdmi HDMI Jack as /devices/platform/sound-hdmi/sound/card1/input1
[ 3.120604] imx8mq-pinctrl 30330000.iomuxc: pin MX8MQ_IOMUXC_NAND_CE2_B already requested by ptn36043; cannot claim for
0-0050
[ 3.132021] imx8mq-pinctrl 30330000.iomuxc: pin-64 (0-0050) status -22
[ 3.138562] imx8mq-pinctrl 30330000.iomuxc: could not request pin 64 (MX8MQ_IOMUXC_NAND_CE2_B) from group typecgrp on d
evice 30330000.iomuxc
[ 3.151272] tcpci 0-0050: Error applying setting, reverse things back
[ 3.157736] tcpci: probe of 0-0050 failed with error -22
[ 3.164065] imx-spdif sound-spdif: ASoC: failed to init link S/PDIF PCM: -517
[ 3.171575] imx-spdif sound-hdmi-arc: ASoC: failed to init link S/PDIF PCM: -517
[ 3.180284] imx-spdif sound-spdif: ASoC: failed to init link S/PDIF PCM: -517
[ 3.187765] imx-spdif sound-hdmi-arc: ASoC: failed to init link S/PDIF PCM: -517
[ 3.197873] snvs_rtc 30370000.snvs:snvs-rtc-lp: setting system clock to 1970-01-01T00:00:01 UTC (1)
[ 3.202384] mmc1: new ultra high speed SDR104 SDHC card at address aaaa
[ 3.207164] cfg80211: Loading compiled-in X.509 certificates for regulatory database
[ 3.214314] mmcblk1: mmc1:aaaa SC16G 14.8 GiB
[ 3.225796] cfg80211: Loaded X.509 cert 'sforshee: 00b28ddf47aef9cea7'
[ 3.230978] mmcblk1: p1 p2
[ 3.232407] platform regulatory.0: Direct firmware load for regulatory.db failed with error -2
[ 3.237215] imx-spdif sound-spdif: ASoC: failed to init link S/PDIF PCM: -517
[ 3.244370] ALSA device list:
[ 3.251320] imx-spdif sound-hdmi-arc: ASoC: failed to init link S/PDIF PCM: -517
[ 3.253894] platform regulatory.0: Falling back to sysfs fallback for: regulatory.db
[ 3.255659] #0: wm8524-audio
[ 3.255661] #1: imx-audio-hdmi
[ 3.329094] hub 1-1:1.0: USB hub found
[ 3.333920] hub 1-1:1.0: 4 ports detected
[ 3.396558] imx-spdif sound-spdif: ASoC: failed to init link S/PDIF PCM: -517
[ 3.404236] imx-spdif sound-hdmi-arc: ASoC: failed to init link S/PDIF PCM: -517
[ 3.591627] EXT4-fs (mmcblk1p2): recovery complete
[ 3.597050] EXT4-fs (mmcblk1p2): mounted filesystem with ordered data mode. Opts: (null)
[ 3.605372] VFS: Mounted root (ext4 filesystem) on device 179:98.
[ 3.619633] devtmpfs: mounted
[ 3.623395] Freeing unused kernel memory: 2880K
[ 3.627992] Run /sbin/init as init process
[ 3.763123] systemd[1]: System time before build time, advancing clock.
[ 3.786018] systemd[1]: systemd 243.2+ running in system mode. (+PAM -AUDIT -SELINUX +IMA -APPARMOR +SMACK +SYSVINIT +UT
MP -LIBCRYPTSETUP -GCRYPT -GNUTLS +ACL +XZ -LZ4 -SECCOMP +BLKID -ELFUTILS +KMOD -IDN2 -IDN -PCRE2 default-hierarchy=hybrid)
[ 3.807965] systemd[1]: Detected architecture arm64.

Welcome to NXP i.MX Release Distro 5.4-zeus (zeus)!

[ 3.863773] systemd[1]: Set hostname to <imx8mqevk>.
[ 4.060742] systemd[1]: /lib/systemd/system/dbus.socket:5: ListenStream= references a path below legacy directory /var/r
un/, updating /var/run/dbus/system_bus_socket ��→ /run/dbus/system_bus_socket; please update the unit file accordingly.
[ 4.091722] systemd[1]: /lib/systemd/system/syslogd.service:8: PIDFile= references a path below legacy directory /var/ru
n/, updating /var/run/syslogd.pid ��→ /run/syslogd.pid; please update the unit file accordingly.
[ 4.122304] systemd[1]: /lib/systemd/system/rpcbind.socket:5: ListenStream= references a path below legacy directory /va
r/run/, updating /var/run/rpcbind.sock ��→ /run/rpcbind.sock; please update the unit file accordingly.
[ 4.148416] systemd[1]: /lib/systemd/system/klogd.service:8: PIDFile= references a path below legacy directory /var/run/
, updating /var/run/klogd.pid ��→ /run/klogd.pid; please update the unit file accordingly.
[ 4.265358] systemd[1]: system-getty.slice: unit configures an IP firewall, but the local system does not support BPF/cg
roup firewalling.
[ 4.277777] systemd[1]: (This warning is only shown for the first unit using IP firewalling.)
[ 4.288085] systemd[1]: Created slice system-getty.slice.
[ OK ] Created slice system-getty.slice.
[ OK ] Created slice system-serial\x2dgetty.slice.
[ OK ] Created slice User and Session Slice.
[ OK ] Started Dispatch Password ��…ts to Console Directory Watch.
[ OK ] Started Forward Password R��…uests to Wall Directory Watch.
[ OK ] Reached target Host and Network Name Lookups.
[ OK ] Reached target Paths.
[ OK ] Reached target Remote File Systems.
[ OK ] Reached target Slices.
[ OK ] Reached target Swap.
[ OK ] Listening on Syslog Socket.
[ OK ] Listening on initctl Compatibility Named Pipe.
[ OK ] Listening on Journal Audit Socket.
[ OK ] Listening on Journal Socket (/dev/log).
[ OK ] Listening on Journal Socket.
[ OK ] Listening on Network Service Netlink Socket.
[ OK ] Listening on udev Control Socket.
[ OK ] Listening on udev Kernel Socket.
Mounting Huge Pages File System...
Mounting POSIX Message Queue File System...
Mounting Kernel Debug File System...
Mounting Temporary Directory (/tmp)...
Starting Create list of st��…odes for the current kernel...
Starting Journal Service...
Mounting Kernel Configuration File System...
Starting Remount Root and Kernel File Systems...
Starting Apply Kernel Variables...
Starting udev Coldplug all Devices...
Starting Setup Virtual Console...
[ OK ] Started Journal Service.
[FAILED] Failed to mount Huge Pages File System.
See 'systemctl status dev-hugepages.mount' for details.
[FAILED] Failed to mount POSIX Message Queue File System.
See 'systemctl status dev-mqueue.mount' for details.
[FAILED] Failed to mount Kernel Debug File System.
See 'systemctl status sys-kernel-debug.mount' for details.
[FAILED] Failed to mount Temporary Directory (/tmp).
See 'systemctl status tmp.mount' for details.
[DEPEND] Dependency failed for Login Service.
[DEPEND] Dependency failed for Network Time Synchronization.
[ OK ] Started Create list of sta��… nodes for the current kernel.
[FAILED] Failed to mount Kernel Configuration File System.
See 'systemctl status sys-kernel-config.mount' for details.
[FAILED] Failed to start Remount Root and Kernel File Systems.
See 'systemctl status systemd-remount-fs.service' for details.
[ OK ] Started Apply Kernel Variables.
[ OK ] Started Setup Virtual Console.
[ OK ] Reached target System Time Set.
[ OK ] Reached target System Time Synchronized.
Starting Flush Journal to Persistent Storage...
[ 5.138178] systemd-journald[250]: Received client request to flush runtime journal.
Starting Create Static Device Nodes in /dev...
[ OK ] Started Flush Journal to Persistent Storage.
[ OK ] Started Create Static Device Nodes in /dev.
[ OK ] Reached target Local File Systems (Pre).
Mounting /var/volatile...
Starting udev Kernel Device Manager...
[ OK ] Started udev Coldplug all Devices.
[FAILED] Failed to mount /var/volatile.
See 'systemctl status var-volatile.mount' for details.
[DEPEND] Dependency failed for Bind mount volatile /srv.
[DEPEND] Dependency failed for Bind mount volatile /var/cache.
[DEPEND] Dependency failed for Bind mount volatile /var/spool.
[DEPEND] Dependency failed for Bind mount volatile /var/lib.
[DEPEND] Dependency failed for Local File Systems.
[ OK ] Started udev Kernel Device Manager.
[ OK ] Stopped Dispatch Password ��…ts to Console Directory Watch.
[ OK ] Stopped Forward Password R��…uests to Wall Directory Watch.
[ OK ] Reached target Timers.
[ OK ] Reached target Network (Pre).
Starting Start Psplash Boot Screen...
[ OK ] Reached target Login Prompts.
[ OK ] Closed Syslog Socket.
Starting Network Service...
Starting Load/Save Random Seed...
[ OK ] Reached target Sockets.
[ OK ] Started Emergency Shell.
[ OK ] Reached target Emergency Mode.
Starting Create Volatile Files and Directories...
[ OK ] Started Network Service.
[ OK ] Started Start Psplash Boot Screen.
[ OK ] Started Load/Save Random Seed.
[ OK ] Started Create Volatile Files and Directories.
[ OK ] Created slice system-weston.slice.
[ OK ] Started Dispatch Password ��…ts to Console Directory Watch.
[ OK ] Stopped target Emerg[ 5.777831] imx-sdma 30bd0000.dma-controller: loaded firmware 4.5
ency Mode.
[ OK ] Reached target Network.
[ OK ] Reached target Sound Card.
Mounting Huge Pages File System...
[ 5.841878] Atheros 8031 ethernet 30be0000.ethernet-1:00: attached PHY driver [Atheros 8031 ethernet] (mii_bus:phy_addr=
30be0000.ethernet-1:00, irq=POLL)
Mounting POSIX Message Queue File System...
Mounting Kernel Debug File System...
Mounting Temporary Directory (/tmp)...
Mounting /var/volatile...
Mounting Kernel Configuration File System...
Starting Remount Root and Kernel File Systems...
[ OK ] Stopped Emergency Shell.
[FAILED] Failed to mount Huge Pages File System.
See 'systemctl status dev-hugepages.mount' for details.
[FAILED] Failed to mount POSIX Message Queue File System.
See 'systemctl status dev-mqueue.mount' for details.
[FAILED] Failed to mount Kernel Debug File System.
See 'systemctl status sys-kernel-debug.mount' for details.
[FAILED] Failed to mount Temporary Directory (/tmp).
See 'systemctl status tmp.mount' for details.
[DEPEND] Dependency failed for Network Time Synchronization.
[FAILED] Failed to mount /var/volatile.
See 'systemctl status var-volatile.mount' for details.
[DEPEND] Dependency failed for Bind mount volatile /srv.
[DEPEND] Dependency failed for Bind mount volatile /var/cache.
[DEPEND] Dependency failed for Bind mount volatile /var/spool.
[DEPEND] Dependency failed for Bind mount volatile /var/lib.
[DEPEND] Dependency failed for Local File Systems.
[FAILED] Failed to mount Kernel Configuration File System.
See 'systemctl status sys-kernel-config.mount' for details.
[FAILED] Failed to start Remount Root and Kernel File Systems.
See 'systemctl status systemd-remount-fs.service' for details.
[ OK ] Created slice system-systemd\x2dfsck.slice.
[ OK ] Stopped Dispatch Password ��…ts to Console Directory Watch.
Starting File System Check on /dev/mmcblk1p1...
[ OK ] Started Emergency Shell.
[ OK ] Reached target Emergency Mode.
Starting Update UTMP about System Boot/Shutdown...
[ OK ] Started Update UTMP about System Boot/Shutdown.
Starting Update UTMP about System Runlevel Changes...
[ OK ] Started Update UTMP about System Runlevel Changes.
[ OK ] Started File System Check on /dev/mmcblk1p1.
Mounting /run/media/mmcblk1p1...
[FAILED] Failed to mount /run/media/mmcblk1p1.
See 'systemctl status run-media-mmcblk1p1.mount' for details.
You are in emergency mode. After logging in, type "journalctl -xb" to view
system logs, "systemctl reboot" to reboot, "systemctl default" or "exit"
to bootPress Enter for maintenance
(or press Control-D to continue):
sh-5.0#

 

I don't think superuser permission is working.

 

regards!

0 件の賞賛
返信
1 解決策
5,150件の閲覧回数
kangmw086
Contributor III

Thank you for your answer.

It seems that an error occurred during the YOCTO build process.

It deleted all the zeus versions and started fresh in the repo phase to confirm normal booting.

 

regards.

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
5,177件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi kangmw086

 

from log : "Failed to mount /run/media/mmcblk1p1" seems there may be problem

with sd port used in kernel boot parameters,  one can check

Table 54. Linux uSDHC relationships i.MX Linux User’s Guide​

 

Best regards
igor

0 件の賞賛
返信
5,151件の閲覧回数
kangmw086
Contributor III

Thank you for your answer.

It seems that an error occurred during the YOCTO build process.

It deleted all the zeus versions and started fresh in the repo phase to confirm normal booting.

 

regards.

0 件の賞賛
返信