[imx8mq] wifi<----->wifi mode support

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

[imx8mq] wifi<----->wifi mode support

1,034 Views
jhii6488_vine
Contributor I

I am using Atheros QCA9882 chipset(wle600v5-27), driver is ath10k. When I printed out the mode supported by wifi on the board, it was as follows.

-------------------------------------------------------------------------------
WIFI-PROPERTIES.WEP: yes
WIFI-PROPERTIES.WPA: yes
WIFI-PROPERTIES.WPA2: yes
WIFI-PROPERTIES.TKIP: yes
WIFI-PROPERTIES.CCMP: yes
WIFI-PROPERTIES.AP: yes
WIFI-PROPERTIES.ADHOC: no
WIFI-PROPERTIES.2GHZ: no
WIFI-PROPERTIES.5GHZ: yes
WIFI-PROPERTIES.MESH: yes
WIFI-PROPERTIES.IBSS-RSN: yes
-------------------------------------------------------------------------------

 

If I want to communicate with wifi<----->wifi other than mesh mode, can you tell me what can I do?

However, I cannot use Access Point <-----> Station mode.

0 Kudos
Reply
1 Reply

1,028 Views
igorpadykov
NXP Employee
NXP Employee

Hi Hyein

 

unfortunately QCA9882 is not supported in NXP BSPs, supported devices are listed

in sect.11.1 Connectivity for Bluetooth wireless technology and Wi-Fi   i.MX Linux User’s Guide​

One can look at ath10k driver description below

https://wireless.wiki.kernel.org/en/users/drivers/ath10k

and post issue (if necessary) on linux wireless mailing list

https://wireless.wiki.kernel.org/en/developers/mailinglists

 

Best regards
igor

0 Kudos
Reply