imx8mq qt5 zxdg_shell_v6

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

imx8mq qt5 zxdg_shell_v6

1,272 次查看
kangmw086
Contributor III

hi.

use info.

imx8mq, yocto rocko,  linux imx8mqevk 4.9.88-imx_4.9.88_2.0.0_ga+g5e23f9d.

qt5.9.4 used.

When you run qt5 application, it works fine.

However, the value of the qt application's combox is not selected.

If you click on combox and select another area, the application dies with the following error:

zxdg_shell_v6@19: error 2: xdg_popup was not created on the topmost popup
The Wayland connection experienced a fatal error (Protocol error)

 

Is it solvable?

标记 (1)
0 项奖励
回复
1 回复

1,268 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello kangmw086,

 

This is a bug in qt appears to be fixed in most recent QT

https://bugreports.qt.io/browse/QTBUG-81952

Please update your yocto with latest version.

 

Regards

 

 

0 项奖励
回复