imx8mq hdmi does not work

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx8mq hdmi does not work

Jump to solution
1,421 Views
1541189572
Contributor III

linux kernel version Linux version 4.14.98-imx_4.14.98_2.0.0_ga+g5d6cbeafb80c. 

the boot log about hdmi:

root@imx8mqevk:~# dmesg | grep hdmi
[ 4.028982] imx-spdif sound-hdmi-arc: snd-soc-dummy-dai <-> 308a0000.spdif mapping ok
[ 4.036839] imx-spdif sound-hdmi-arc: ASoC: no DMI vendor name!
[ 4.108431] imx-cdnhdmi sound-hdmi: ASoC: CODEC DAI i2s-hifi not registered
[ 4.115468] imx-cdnhdmi sound-hdmi: snd_soc_register_card failed (-517)
[ 4.806502] imx-cdnhdmi sound-hdmi: ASoC: CODEC DAI i2s-hifi not registered
[ 4.813554] imx-cdnhdmi sound-hdmi: snd_soc_register_card failed (-517)
[ 4.857804] #2: imx-hdmi-arc
root@imx8mqevk:~# dmesg | grep dcss
[ 1.009618] dcss-core 32e00000.dcss: failed to get pix clock
[ 1.015299] dcss-core 32e00000.dcss: clocks initialization failed
[ 1.021413] dcss-core: probe of 32e00000.dcss failed with error -2
Labels (1)
0 Kudos
1 Solution
1,232 Views
1541189572
Contributor III

Solved!  4.14.98-imx_4.14.98_2.0.0_ga kernel should use  the corresponded device tree. I used  4.14.78 version device tree which does not include pix clock in the device tree.

View solution in original post

0 Kudos
1 Reply
1,233 Views
1541189572
Contributor III

Solved!  4.14.98-imx_4.14.98_2.0.0_ga kernel should use  the corresponded device tree. I used  4.14.78 version device tree which does not include pix clock in the device tree.

0 Kudos