hi NXP
we are using SAMSUNG 4k tv (version BA01 supports HDR ) with IMX8mq-evk
the hdmi is not working and xwayland window is not coming on the tv
showing hdmi plug in and hdmi plug out error on console
the tv is detecting the device connected to it .like PC and settop box etc
but the IMx8evk is not being detected by the tv and saying unknown device ?
could you please support us to resole this ? what could be wrong ?
we are using yocto xwayland image
note: old samsung 4k tv is working with imx8mq-evk
regards
Nagendra
Hi Bio,
thanks for suggestion, I tried with all ports available with TV and unfortunately none of them working
the new samsung tv is detecting the hdmi device connected to it. (like PC and settp box etc)
do we need to enable anything to support this detection in IMX hdmi-fw or hdmi driver ?
fyi: also tried with disabling CEC ,hdcp options on imx side
regards,
Nagendra
Hi nagendra,
I just can say to try to connect on another port, there is no report that MX8M works on one 4K Monitor and other no.