I have trouble with this.
My board's options are 0010 (for eMMC boot) and 01 (for serial download mode)
I connected board to my window by usb connector.
This is "mfgtool2-yocto-mx8-evk-emmc1.vbs" in mfgtools-with-rootfs folder.
< Device Manager >
< HyperTerminal Connection >
< MfgTool.log >
DLL version: 2.7.0
Thursday, July 26, 2018 18:27:06 Start new logging
ModuleID[2] LevelID[10]: CMyExceptionHandler thread is running
ModuleID[2] LevelID[1]: new MxHidDeviceClass
ModuleID[2] LevelID[1]: new MxHidDeviceClass
ModuleID[2] LevelID[1]: new MxHidDeviceClass
ModuleID[2] LevelID[10]: DeviceTypeDisk--_devices size: 2
ModuleID[2] LevelID[10]: Volume--StorageDisk, Disk->_driveNumber:3, Volume->_diskNumber:2
ModuleID[2] LevelID[10]: Volume--StorageDisk, Disk->_driveNumber:2, Volume->_diskNumber:2
ModuleID[2] LevelID[10]: DeviceTypeDisk--find Disk device: 00C67DB0
ModuleID[2] LevelID[10]: DeviceTypeDisk--_devices size: 2
ModuleID[2] LevelID[10]: Volume--StorageDisk, Disk->_driveNumber:3, Volume->_diskNumber:3
ModuleID[2] LevelID[10]: DeviceTypeDisk--find Disk device: 00C543D8
ModuleID[2] LevelID[10]: Device::hubIndex::getmsc, return the port index is: 10
ModuleID[2] LevelID[10]: Device Manager thread is running
ModuleID[2] LevelID[1]: Can't set m_hStopEvent before it initialized or it already stop
ModuleID[2] LevelID[10]: CCmdOpreation[0] thread is Closed
ModuleID[2] LevelID[10]: CCmdOpreation[0] thread is Closed
ModuleID[2] LevelID[10]: DeviceManager::OnMsgDeviceEvent() - EVENT_KILL
ModuleID[2] LevelID[10]: CMyExceptionHandler::OnMsgExceptionEvent() - KillExceptionHandlerThread
ModuleID[2] LevelID[10]: Exception Handler thread is closed
ModuleID[2] LevelID[1]: delete MxHidDeviceClass
ModuleID[2] LevelID[10]: Device Manager thread is closed
Hi Sehan
please check that correct (usb otg, usb cable type C to PC) port was used and set
EVK in Serial Download mode using switch settings, look at MX 8M EVK Board Hardware User's Guide
https://www.nxp.com/docs/en/user-guide/IMX8MDQLQEVKHUG.pdf
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Should I use usb otg or C type?
from board to laptop?
I checked Serial Download mode.
Or.. is there other steps before connect this?
I didn't do anything after I bought this.
Just install driver for this connection from here(Virtual COM Port Drivers )
please check video Getting Started with the i.MX 8M Evaluation Kit
Getting Started with the i.MX 8M Evaluation Kit|NXP
Best regards
igor