imx8mq csi raw10 rx problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx8mq csi raw10 rx problem

3,173 Views
martinkepplinge
Contributor II

I try to capture mipi raw10 data from a sensor (so probably 5 bytes are 4 pixels) in bayer. the mxc-mipi-csi2_yav driver should be no problem afaik.
I apply the following to the mx6s_capture.c csi driver:

--- a/drivers/media/platform/mxc/capture/mx6s_capture.c
+++ b/drivers/media/platform/mxc/capture/mx6s_capture.c
@@ -266,6 +266,12 @@ static struct mx6s_fmt formats[] = {
    .pixelformat = V4L2_PIX_FMT_SBGGR8,
    .mbus_code = MEDIA_BUS_FMT_SBGGR8_1X8,
    .bpp = 1,
+   }, {
+   .name = "RAWRGB10 (SBGGR10)",
+   .fourcc = V4L2_PIX_FMT_SBGGR10,
+   .pixelformat = V4L2_PIX_FMT_SBGGR10,
+   .mbus_code = MEDIA_BUS_FMT_SBGGR10_1X10,
+   .bpp = 2,
    }
    };

@@ -601,6 +607,10 @@ static void csi_set_imagpara(struct mx6s_csi_dev *csi,
{
    int imag_para = 0;
    unsigned long cr3 = __raw_readl(csi->regbase + CSI_CSICR3);
+   int rx_count;
+
+   rx_count = (width * height) >> 2;
+   __raw_writel(rx_count, csi->regbase + CSI_CSIRXCNT);

   imag_para = (width << 16) | height;
   __raw_writel(imag_para, csi->regbase + CSI_CSIIMAG_PARA);
@@ -838,6 +848,7 @@ static int mx6s_configure_csi(struct mx6s_csi_dev *csi_dev)
    switch (csi_dev->fmt->pixelformat) {
    case V4L2_PIX_FMT_YUV32:
    case V4L2_PIX_FMT_SBGGR8:
+   case V4L2_PIX_FMT_SBGGR10:
    width = pix->width;
    break;
    case V4L2_PIX_FMT_UYVY:
@@ -857,7 +868,6 @@ static int mx6s_configure_csi(struct mx6s_csi_dev *csi_dev)
    if (csi_dev->csi_mipi_mode == true) {
    cr1 = csi_read(csi_dev, CSI_CSICR1);
    cr1 &= ~BIT_GCLK_MODE;
-   csi_write(csi_dev, cr1, CSI_CSICR1);

    cr18 = csi_read(csi_dev, CSI_CSICR18);
    cr18 &= ~BIT_MIPI_DATA_FORMAT_MASK;
@@ -871,12 +881,17 @@ static int mx6s_configure_csi(struct mx6s_csi_dev *csi_dev)
    case V4L2_PIX_FMT_SBGGR8:
    cr18 |= BIT_MIPI_DATA_FORMAT_RAW8;
    break;
+   case V4L2_PIX_FMT_SBGGR10:
+   cr18 |= BIT_MIPI_DATA_FORMAT_RAW10;
+   cr1 |= BIT_PIXEL_BIT;
+   break;
    default:
    pr_debug(" fmt not supported\n");
    return -EINVAL;
    }

    csi_write(csi_dev, cr18, CSI_CSICR18);
+   csi_write(csi_dev, cr1, CSI_CSICR1);
    }
    return 0;
    }
@@ -2002,7 +2017,7 @@ static const struct mx6s_csi_soc mx6sl_soc = {
    };
    static const struct mx6s_csi_soc mx8mq_soc = {
    .rx_fifo_rst = true,
-    .baseaddr_switch = 0x80030,
+    .baseaddr_switch = 0x80000,
    };

you can see I switched baseaddr switch from "vsync" to "atomically by DMA completed" because I don't get EOF (or the appropriate) interrupts for vsync.

the dts description for csi1 I:


mipi_csi_1: mipi_csi1@30a70000 {
compatible = "fsl,mxc-mipi-csi2_yav";
reg = <0x30a70000 0x1000>; /* MIPI CSI1 Controller base addr */
interrupts = <GIC_SPI 44 IRQ_TYPE_LEVEL_HIGH>;
clocks = <&clk IMX8MQ_CLK_CSI1_CORE>,
<&clk IMX8MQ_CLK_CSI1_ESC>,
<&clk IMX8MQ_CLK_CSI1_PHY_REF>,
<&clk IMX8MQ_CLK_CLKO2>;
clock-names = "clk_core", "clk_esc", "clk_pxl", "clk_clko2";
assigned-clocks = <&clk IMX8MQ_CLK_CSI1_CORE>,
<&clk IMX8MQ_CLK_CSI1_PHY_REF>,
<&clk IMX8MQ_CLK_CSI1_ESC>;
assigned-clock-rates = <266000000>, <150000000>, <66000000>;
assigned-clock-parents = <&clk IMX8MQ_SYS1_PLL_266M>,
<&clk IMX8MQ_SYS2_PLL_1000M>,
<&clk IMX8MQ_SYS1_PLL_800M>;
power-domains = <&pgc_mipi_csi1>;
csis-phy-reset = <&src 0x4c 7>;
phy-gpr = <&iomuxc_gpr 0x88>;
status = "okay";

port {
#address-cells = <1>;
#size-cells = <0>;
mipi1_sensor_ep: endpoint@1 {
reg = <1>;
remote-endpoint = <&camera1_ep>;
data-lanes = <1 2>;
};

csi1_mipi_ep: endpoint@2 {
reg = <2>;
remote-endpoint = <&csi1_ep>;
};
};
};

csi1_bridge: csi1_bridge@30a90000 {
compatible = "fsl,imx8mq-csi", "fsl,imx6s-csi";
reg = <0x30a90000 0x10000>;
interrupts = <GIC_SPI 42 IRQ_TYPE_LEVEL_HIGH>;
clocks = <&clk IMX8MQ_CLK_DUMMY>,
<&clk IMX8MQ_CLK_CSI1_ROOT>,
<&clk IMX8MQ_CLK_DUMMY>;
clock-names = "disp-axi", "csi_mclk", "disp_dcic";
power-domains = <&pgc_mipi_csi1>;
interconnects = <&noc IMX8MQ_ICM_CSI1 &noc IMX8MQ_ICS_DRAM>;
fsl,mipi-mode;
status = "okay";

port{
csi1_ep: endpoint {
remote-endpoint = <&csi1_mipi_ep>;
};
};
};


the sensor driver uses MEDIA_BUS_FMT_SBGGR10_1X10. now CSI says raw10 to be (converted?) and padded to 16bits per pixel, so I used 2bpp in mx6s_capture.c.

When capturing one frame of 640x480 now, the size is indeed 2x640x480 bytes but it's actually 2 frames concatinated, with each one having obviously 1byte per pixel. (Therefore of course the data is not correct too because the sensor sends raw10):

v4l2-ctl -d 0 --set-fmt-video=width=640,height=480,pixelformat=BG10
v4l2-ctl -d 0 --stream-mmap --stream-to=640.raw --stream-count=1

I attach `hexdump -v 640.raw > 640.raw.txt` and the png of it.


What can I do for RAW10 to be correctly processed by mipi and the csi bridge? Is anything missing here? thank you very much in advance!

Labels (2)
0 Kudos
Reply
7 Replies

3,113 Views
joanxie
NXP TechSupport
NXP TechSupport

+   .name = "RAWRGB10 (SBGGR10)",
+   .fourcc = V4L2_PIX_FMT_SBGGR10,
+   .pixelformat = V4L2_PIX_FMT_SBGGR10,
+   .mbus_code = MEDIA_BUS_FMT_SBGGR10_1X10,
+   .bpp = 2,

how about setting bpp=1? and don't forget enable two-8bit-sensor-mode in the dts file

0 Kudos
Reply

3,078 Views
martinkepplinge
Contributor II

thank you. that helped. 2bpp is indeed needed and shows a "correct" frame, with two-8bit-mode.

note that we had to fix the hardcoded 640x960 that's set in mx6s_capture to instead reflect the actual mode.

one problem persists though: the color range is not correct. white is grey and black is not fully black. see the attached raw file of 640x480 with a color bars test pattern.

0 Kudos
Reply

3,073 Views
joanxie
NXP TechSupport
NXP TechSupport

why did you set baseaddr_switch to 0? which mean set BASEADDR_SWITCH_EN = 0, not care BASEADDR_SWITCH_SEL. The frame buffer only used one and the data is refresh by the embedded DMA. This is not used in the driver; but we have tested that the best way to set 0x80030, how about set to the default value 0x80030?

0 Kudos
Reply

3,068 Views
martinkepplinge
Contributor II

absolutely. that's really only been for testing purposes. for correct modes, the default setting is even needed in order to all frames to be correctly in-sync. That's unrelated to a reduced color-space we currently see though.

Thanks a lot for having a look here.

0 Kudos
Reply

3,163 Views
martinkepplinge
Contributor II

to follow up, here's what I receive in 1280x720 mode: the second frame isn't complete:

 

 

0 Kudos
Reply

3,047 Views
joanxie
NXP TechSupport
NXP TechSupport

let me update, your first question is about you set 640x480, but you get 2x640x480, then you fix this issue when you set bpp=1, right? now the new issue is that you couldn't get the completed second frame and correct color when you set 1280x720 frame size? right?

0 Kudos
Reply

3,043 Views
martinkepplinge
Contributor II

oh thanks for asking! no, 2bpp is definitely correct for a 10-bit bayer format. it obviously doesn't fit into 1bpp and when looking at the data, it looks like correctly padded to 16bit. your previous answer helped. I didn't know that two-8bit is correct in that case (although it *is* mentioned correctly in the RM now that I know it

the size-issue could be resolved: previously  I called the problem "not completed second frame". with 2bpp it's "not completed frame": "imag_para = (640 << 16) | 960;" was hard-coded and changing that to the actual size (allowing more data) fixes the problem.

for the color-issue I'm actually not even sure anymore: "v4l2-ctl --stream-to-host" and viewing with "qvidcap -p" on the host gives correct colors. Does that "debayer only" (and no other post-processing of the color space)? I'm not even sure yet.

to sum up: This ticket can actually be marked as resolved. I face minor other issues I could open new tickets for.

0 Kudos
Reply