imx8mq could not bootup without tee.bin

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx8mq could not bootup without tee.bin

626 Views
jiangyaqiang
Contributor IV

Hi anyone:

   I face a problem , my board could not bootup without tee.bin.

   Here is the information of my board:

   cpu: imx8mq

   system: yocto-4.14.62

    

    test:

    remove file tee.bin in imx-mkimage/iMX8M/tee.bin

    (It's no problem if don't remove the file)

    build: make SOC=iMX8M flash_hdmi_spl_uboot

    

    log:

    
U-Boot SPL 2018.03-00792-g7fac6b9-dirty (Aug 20 2020 - 16:11:07 +0800)
Can't find PMIC:PFUZE100
start to config phy: p0=3200mts, p1=667mts with 1D2D training
check ddr4_pmu_train_imem code
check ddr4_pmu_train_imem code pass
check ddr4_pmu_train_dmem code
check ddr4_pmu_train_dmem code pass
config to do 3200 1d training.
Training PASS
check ddr4_pmu_train_imem code
check ddr4_pmu_train_imem code pass
check ddr4_pmu_train_dmem code
check ddr4_pmu_train_dmem code pass
config to do 3200 2d training.
Training PASS
check ddr4_pmu_train_imem code
check ddr4_pmu_train_imem code pass
check ddr4_pmu_train_dmem code
check ddr4_pmu_train_dmem code pass
pstate=1: set dfi clk done done
Training PASS
Load 201711 PIE
Normal Boot
Trying to boot from MMC1 

(stop here)

0 Kudos
1 Reply

594 Views
igorpadykov
NXP Employee
NXP Employee

Hi Jiang

one can build image without OpTee using sect.5.6.10 OP-TEE enablement

Yocto Guide included in linux Documentation

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos