[imx8mq][android12] How to enable qmi_wwan at /sys/bus/usb/drivers?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

[imx8mq][android12] How to enable qmi_wwan at /sys/bus/usb/drivers?

Jump to solution
6,297 Views
fengyingchu
Contributor II

I can enable option and usbserial drivers at /sys/bus/usb/drivers; however, how to enable qmi_wwan at /sys/bus/usb/drivers?

I added the following at the file: imx8mq_ima_gki.fragment

+CONFIG_PPP_ASYNC=m
+CONFIG_PPP_SYNC_TTY=m
+CONFIG_USBNET=m
+CONFIG_USB_USBNET=m
+CONFIG_USB_WDM=m
+CONFIG_USB_NET_QMI_WWAN=m
+CONFIG_USB_SERIAL_QUALCOMM=m

And I added the following at the file: imx_v8_ima_android_defconfig

+CONFIG_PPP_ASYNC=y
+CONFIG_PPP_SYNC_TTY=y
+CONFIG_USBNET=y
+CONFIG_USB_WDM=y
+CONFIG_USB_NET_QMI_WWAN=y
+CONFIG_USB_SERIAL_QUALCOMM=y

And I added the following at the file: SharedBoardConfig.mk

$(KERNEL_OUT)/drivers/usb/serial/usbserial.ko \
$(KERNEL_OUT)/drivers/usb/serial/usb_wwan.ko \
$(KERNEL_OUT)/drivers/usb/serial/option.ko \
$(KERNEL_OUT)/drivers/usb/serial/qcserial.ko \
$(KERNEL_OUT)/drivers/net/usb/qmi_wwan.ko \
$(KERNEL_OUT)/drivers/net/ppp/ppp_async.ko \
$(KERNEL_OUT)/drivers/net/ppp/ppp_synctty.ko \
$(KERNEL_OUT)/drivers/net/usb/usbnet.ko

As the above settings, I can build and flash to the device successfully.

After flashing, I can see there are option.ko and qmi_wwan.ko in the device.

-rw-r--r-- 1 root root 185440 2023-02-07 10:46 ./vendor/lib/modules/option.ko
-rw-r--r-- 1 root root 105744 2023-02-07 10:46 ./vendor/lib/modules/qmi_wwan.ko

And when I check  the path /sys/bus/usb/drivers, I just saw option driver. I cannot get qmi_wwan driver.

Could you please help me to clarify this issue? Thanks a lot.

0 Kudos
Reply
1 Solution
6,201 Views
fengyingchu
Contributor II

Hi, 

This issue has been solved. It can be closed.

I just moved some codes to qmi_wwan.c and cdc_wdm.c. It is ok to have the module of qmi_wwan and cdc_wdm. Thanks a lot.

View solution in original post

0 Kudos
Reply
5 Replies
6,280 Views
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hello @fengyingchu 

The qmi_wwan driver is suitable for Qualcomm SOC, not i.MX

0 Kudos
Reply
6,248 Views
fengyingchu
Contributor II

Hi, I use the imx SOC with Quectel GPS and LTE.

The driver of Quectel GPS and LTE needs to use qmi_wwan driver.

0 Kudos
Reply
6,239 Views
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Have you tried to install the driver manually?

0 Kudos
Reply
6,202 Views
fengyingchu
Contributor II

Hi, 

This issue has been solved. It can be closed.

I just moved some codes to qmi_wwan.c and cdc_wdm.c. It is ok to have the module of qmi_wwan and cdc_wdm. Thanks a lot.

0 Kudos
Reply
6,231 Views
fengyingchu
Contributor II

Hi,

I did "insmod ./vendor/lib/modules/qmi_wwan.ko", and the dmesg log shows: "Unknown symbol usb_cdc_wdm_register (err -2)".

Then, I did "insmod ./vendor/lib/modules/cdc-wdm.ko", and the dmesg log shows "Unknown symbol usb_register_dev (err -2)".

However, I don't know how to solve usb_register_dev problem, because I cannot build usbcore.ko out.

I think the build system do not allow me to set CONFIG_USB to be m.

The attachments are the dmesg log and my .config file.

Thanks.

0 Kudos
Reply