Hi Igor,
Thanks for reply. Yes board pass DDR init as same image can boot from emmc and we generate ddr training from official nxp memory tool.
I checked fuses and it says:
USDHC_PAD_SET
TINGS
0x490[31:24]
NAND_PAD_SETT
IN GS
0x4A0[31:24]
OEM Override values for
the SD/MMC and
NAND boot modes
No 00000000 Override the
following IO PAD
settings:
[1:0] Driver
Strength
[2] Slew Rate
[3] Hysteresis
[4] Pull/Keeper
select
[6:5] Pull up/down
config
[7] Reserved.
USDHC_OVERRID
E_PAD_SETTING
S
0x490[17]
OEM Overrides the HYS
bit for the SD pads
No 0 Override the IO
so it's for pads configs (pull up/down etc) but can I change pinmux of pin like attach it to alt config or so? Thanks.