Dear NXP ,
HW : imx8mplus
u-boot version : 2021.04-r0
kernel version : 5.10.72
Secure boot :
step 1 :
$ hexdump -e '/4 "0x"' -e '/4 "%X""\n"' SRK_1_2_3_4_fuse.bin
0x1BEBF778
0x3CEB2A
0xC41D3D61
0xD55165F3
0x70A014A9
0x1852CC22
0xED495390
0x488C0B93
step 2:
fuse prog 6 0 0x1BEBF778
fuse prog 6 1 0x3CEB2A
fuse prog 6 2 0xC41D3D61
fuse prog 6 3 0xD55165F3
fuse prog 7 0 0x70A014A9
fuse prog 7 1 0x1852CC22
fuse prog 7 2 0xED495390
fuse prog 7 3 0x488C0B93
step 3:
- Program SRK_LOCK:
=> fuse prog 0 0 0x200
- Program DIR_BT_DIS:
=> fuse prog 1 3 0x8000000
- Program SJC_DISABLE:
=> fuse prog 1 3 0x200000
- JTAG_SMODE:
=> fuse prog 1 3 0xC00000
step 4:
fuse prog 1 3 0x02000000
Refer to the picture below. This srg-imx8mplus platform has started secure boot, and Authenticate kernel image fail. Please check message after booting. I think the uboot authentication is passed.
Just to load kernel image failed.
I found out that setp3 is not needed . I want to know if imx8mplus secure boot only choose
verify u-boot signed image. Is this OK ?
Is it necessary to verify kernel and rootfs images?
Dear NXP ,
I add some debug message in hab.c. In u-boot mode , it show meaasge as follows:
### [authenticate_image] ###
ddr_start : 0x40480000
ivt_offset : 0x1d90000
IVT_SIZE : 0x20
CSF_PAD_SIZE : 0x2000
bytes : 0x1d92020
refer to the imx_hab_authenticate_image(ddr_start, bytes, ivt_offset);
Run command as follows:
hab_auth_img 0x40480000 0x1d92020 0x1d90000
Please help fix this issue .
hab_auth_img 0x40480000 0x1CD9A00 0x20
It seems the 3rd parameter ivt offset 0x20 is wrong.
you can add debug information here to make sure all the parameters match your wish.
u-boot/arch/arm/mach-imx/hab.c
int authenticate_image(u32 ddr_start, u32 raw_image_size)
{
u32 ivt_offset;
size_t bytes;
ivt_offset = (raw_image_size + ALIGN_SIZE - 1) &
~(ALIGN_SIZE - 1);
bytes = ivt_offset + IVT_SIZE + CSF_PAD_SIZE;
return imx_hab_authenticate_image(ddr_start, bytes, ivt_offset);
}
Hi @t2865k5
(1) How to only choose to verify u-boot without verifying the kernel image ?
You can disable kernel verification in uboot.
diff --git a/cmd/booti.c b/cmd/booti.c
index d820930fe8..e1122f3e38 100644
--- a/cmd/booti.c
+++ b/cmd/booti.c
@@ -78,7 +78,8 @@ static int booti_start(struct cmd_tbl *cmdtp, int flag, int argc,
if (ret != 0)
return 1;
-#if defined(CONFIG_IMX_HAB) && !defined(CONFIG_AVB_SUPPORT)
+#if 0
+
extern int authenticate_image(
uint32_t ddr_start, uint32_t raw_image_size);
if (authenticate_image(ld, image_size) != 0) {
(2) I have referred to the mx8m_secure_boot.txt but Authenticating kernel image is failed . Please check the imx8mplusSecureBoot.docx .
Try to authenticate the size for image: Image_pad_ivt.bin
Best regards
Harvey
Hi @t2865k5
I want to know if imx8mplus secure boot only choose verify u-boot signed image. Is this OK ? Is it necessary to verify kernel and rootfs images?
Ans: Mostly depends on your need; I'd recommend sign kernel too.
To the error of additional singing, would suggest to check if you've padded kernel as step: 3.1 Padding the image (uboot-imx/doc/imx/habv4/guides/mx8m_secure_boot.txt at lf_v2022.04 · nxp-imx/uboot-imx · GitHub) and better check again the signing image including ivt.
Best regards
Harvey
Dear NXP ,
Please refer to the csf_additional_images.txt.
cd cst-3.1.0/csf/
../linux64/bin/cst --i csf_additional_images.txt --o csf_kernel.bin
cat Image_pad_ivt.bin csf_kernel.bin > Image_signed
copy uboot , kernel image and imx8mp-evk.dtb to SD card .
I get some error log when imx8mplus boot . Please refer to the picture .
Please help to me to fix this issue .