imx8mp windows10 iot winpe not found emmc

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx8mp windows10 iot winpe not found emmc

204 Views
aber
Contributor III

Hello nxp

     I installed Windows 10 IoT on IMX8MP and was able to find EMMC normally in Uboot. However, I cannot recognize EMMC in Windows PE. Could you please help analyze the reason。Tks!

微信图片_20240625181817.jpg

   u-boot=> mmc dev 2
switch to partitions #0, OK
mmc2(part 0) is current device
u-boot=> mmc info
Device: FSL_SDHC
Manufacturer ID: 15
OEM: 0
Name: BJTD4R
Bus Speed: 50000000
Mode: MMC High Speed (52MHz)
Rd Block Len: 512
MMC version 5.1
High Capacity: Yes
Capacity: 29.1 GiB
Bus Width: 8-bit
Erase Group Size: 512 KiB
HC WP Group Size: 8 MiB
User Capacity: 29.1 GiB WRREL
Boot Capacity: 4 MiB ENH
RPMB Capacity: 4 MiB ENH
Boot area 0 is not write protected
Boot area 1 is not write protected

0 Kudos
Reply
0 Replies