imx8mp vpu encoder: vc8000e: driver segmentation fault

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

imx8mp vpu encoder: vc8000e: driver segmentation fault

103 次查看
vmbtech
Contributor I

0x0000ffffd83ba748 in VCEncStrmEncodeExt () from /lib/libhantro_vc8000e.so.1 (gdb) bt
#0 0x0000ffffd83ba748 in VCEncStrmEncodeExt () from /lib/libhantro_vc8000e.so.1 warning: could not convert 'main' from the host encoding (ANSI_X3.4-1968) to UTF-32. This normally should not happen, please file a bug report.
#1 0x0000ffffd83bdc00 in VCEncStrmEncode () from /lib/libhantro_vc8000e.so.1
#2 0x0000ffffd84e771c in VCEnc_encoder_encode () from /lib/libfslvpuwrap.so.3
#3 0x0000ffffd84e8124 in VPU_EncEncodeFrame () from /lib/libfslvpuwrap.so.3
#4 0x0000ffffd85a2af4 in ?? () from /lib/gstreamer-1.0/libgstvpu.so
#5 0x0000fffff65bf9b8 in ?? () from /lib/libgstvideo-1.0.so.0
#6 0x0000fffff78e43a8 in ?? () from /lib/libgstreamer-1.0.so.0
#7 0x0000fffff78e65bc in ?? () from /lib/libgstreamer-1.0.so.0
#8 0x0000fffff78ee6f4 in gst_pad_push () from /lib/libgstreamer-1.0.so.0
#9 0x0000fffff7aba87c in ?? () from /lib/libgstbase-1.0.so.0
#10 0x0000fffff78e43a8 in ?? () from /lib/libgstreamer-1.0.so.0
#11 0x0000fffff78e65bc in ?? () from /lib/libgstreamer-1.0.so.0
#12 0x0000fffff78ee6f4 in gst_pad_push () from /lib/libgstreamer-1.0.so.0
#13 0x0000fffff7aba87c in ?? () from /lib/libgstbase-1.0.so.0
#14 0x0000fffff78e43a8 in ?? () from /lib/libgstreamer-1.0.so.0
#15 0x0000fffff78e65bc in ?? () from /lib/libgstreamer-1.0.so.0
#16 0x0000fffff78ee6f4 in gst_pad_push () from /lib/libgstreamer-1.0.so.0
#17 0x0000ffffd86a6cac in ?? () from /lib/gstreamer-1.0/libgstvideorate.so
#18 0x0000fffff7abaeb0 in ?? () from /lib/libgstbase-1.0.so.0
#19 0x0000fffff7aba7fc in ?? () from /lib/libgstbase-1.0.so.0
#20 0x0000fffff78e43a8 in ?? () from /lib/libgstreamer-1.0.so.0
#21 0x0000fffff78e65bc in ?? () from /lib/libgstreamer-1.0.so.0
#22 0x0000fffff78ee6f4 in gst_pad_push () from /lib/libgstreamer-1.0.so.0
#23 0x0000fffff4218118 in ?? () from /lib/gstreamer-1.0/libgstcoreelements.so
#24 0x0000fffff7923390 in ?? () from /lib/libgstreamer-1.0.so.0
#25 0x0000fffff749e954 in ?? () from /lib/libglib-2.0.so.0
#26 0x0000fffff749dc68 in ?? () from /lib/libglib-2.0.so.0
#27 0x0000fffff72b0d14 in ?? () from /lib/libc.so.6
#28 0x0000fffff731364c in ?? () from /lib/libc.so.6

 

Certain combinations of bitrates, gop size and complexity seem to exarcerbate this.

I would like to fix the segfault at source so I need the source code for the following library:

libhantro_vc8000e.so.1

Is this available anywhere?

0 项奖励
回复
1 回复

71 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

The source code is proprietary you need to check with professional services if you can obtain the source code.

https://www.nxp.com/support/support/nxp-engineering-services/professional-support-for-processors-and...

Regards

 

0 项奖励
回复