imx8mp jailhouse can not boot another kernel:execvp: No such file or directory

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx8mp jailhouse can not boot another kernel:execvp: No such file or directory

752 Views
jimmyhua
Contributor I

uboot boot:run jh_mmcboot

after kernel boot, cd /home/root/jailhouse

jimmyhua_1-1719467256228.png

 

 insmod jailhouse.ko

 

./jailhouse enable ./imx8mp.cell

./jailhouse cell linux ./imx8mp-linux-demo.cell /run/media/mmcblk2p1/Image -d /run/media/mmcblk2p1/imx8mp-evk-inmate.dtb -c "clk_ignore_unused console=ttymxc1,115200 earlycon=ec_imx6q,0x30860000,115200 root=/dev/mmcblk2p2 rootwait rw" print execvp: No such file or directory

jimmyhua_0-1719467180522.png

 

why?./jailhouse cell linux fail

0 Kudos
Reply
1 Reply

731 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

i.MX jailhouse code could be accessed from https://github.com/nxp-imx/imx-jailhouse

jailhouse only support dual linux, linux plus baremetal. If you would run android, you need customize.

Kernel & Virtualization Engineer
Regards
0 Kudos
Reply