imx8mp_evk : the read speed of SAI RDR(n) Register is too low

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx8mp_evk : the read speed of SAI RDR(n) Register is too low

2,164 Views
Chengting
Contributor II

We'd plan to use the SAI interface of imx8mp_evk, for high speed data receive, not for the normal audio usage. But found that the  read speed of SAI RDR(n) Register is too low.

Now we are doing a test of make the SAI1_RX_BCLK = 40 Mhz, 4 data channels(0~3channels)

SAI_RX_SYNX = 40/(32*2), framesize = 64. FIFO mechanism.

But we encountered the FIFO full interrupt.

That means the Read speed is far behind the message receive speed.

And then we take a teat of reading SAI1 RDR register.

 

void test_read_register(void)
{
    SAI_RxEnable(DEMO_SAI, true);
    uint32_t *p_testdata = (uint32_t *)g_data_test;
    int index =0;
    // print_sai_registers(DEMO_SAI);
    PRINTF("SAI example  begin!\n\r");
    int j=0;
    while(index < 100000000)
    {
        p_testdata[j++] = DEMO_SAI->RDR[0];
        index++;
        p_testdata[j++] = DEMO_SAI->RDR[1];
        index++;
        p_testdata[j++] = DEMO_SAI->RDR[2];
        index++;
        p_testdata[j++] = DEMO_SAI->RDR[3];
        index++;
        p_testdata[j++] = DEMO_SAI->RDR[0];
        index++;
        p_testdata[j++] = DEMO_SAI->RDR[1];
        index++;
        p_testdata[j++] = DEMO_SAI->RDR[2];
        index++;
        p_testdata[j++] = DEMO_SAI->RDR[3];
        index++;
        j = 0;

    }
    print_sai_registers(DEMO_SAI);
    // print_sai_registers(DEMO_SAI);
    PRINTF("\n\r SAI example finished! index =%d\n\r",index);

}

 

The Clock configuration could be checked in the attachment.

 

    CLOCK_SetRootMux(kCLOCK_RootSai1, kCLOCK_SaiRootmuxAudioPll1); /* Set SAI source to AUDIO PLL1 393216000HZ*/
    //chengting
    CLOCK_SetRootDivider(kCLOCK_RootSai1, 1U, 1U);                /* Set root clock to 393216000HZ / 16 = 24.576MHz */
void BOARD_BootClockRUN(void)
{
    /* * The following steps just show how to configure the PLL clock sources using the clock driver on M7 core side .
     * Please note that the ROM has already configured the SYSTEM PLL1 to 800Mhz when power up the SOC, meanwhile A core
     * would enable SYSTEM PLL1, SYSTEM PLL2 and SYSTEM PLL3 by U-Boot.
     * Therefore, there is no need to configure the system PLL again on M7 side, otherwise it would have a risk to make
     * the SOC hang.
     */

    /* switch AHB NOC root to 24M first in order to configure the SYSTEM PLL1. */
    CLOCK_SetRootMux(kCLOCK_RootAhb, kCLOCK_AhbRootmuxOsc24M);

    /* switch AXI M7 root to 24M first in order to configure the SYSTEM PLL2. */
    CLOCK_SetRootMux(kCLOCK_RootM7, kCLOCK_M7RootmuxOsc24M);

    // CLOCK_InitSysPll2(&g_sysPll2Config); /* init SYSTEM PLL2 run at 1000MHZ */
    // CLOCK_InitSysPll3(&g_sysPll3Config); /* init SYSTEM PLL3 run at 600MHZ */

    CLOCK_InitAudioPll1(&g_audioPll1Config); /* init AUDIO PLL1 run at 393216000HZ */
    CLOCK_InitAudioPll2(&g_audioPll2Config); /* init AUDIO PLL2 run at 361267200HZ */
    CLOCK_SetRootDivider(kCLOCK_RootM7, 1U, 1U);              /* Set root clock to 800M */
    CLOCK_SetRootMux(kCLOCK_RootM7, kCLOCK_M7RootmuxSysPll1); /* switch cortex-m7 to SYSTEM PLL1 */
    
    // CLOCK_SetRootDivider(kCLOCK_RootQspi, 1U, 2U);              /* Set root clock to 800M */
    // CLOCK_SetRootMux(kCLOCK_RootM7, kCLOCK_M7RootmuxSysPll1); /* switch QSPI to SYSTEM PLL1 */

    CLOCK_SetRootDivider(kCLOCK_RootAhb, 1U, 1U);                   /* Set root clock freq to 133M / 1= 133MHZ */
    CLOCK_SetRootMux(kCLOCK_RootAhb, kCLOCK_AhbRootmuxSysPll1Div6); /* switch AHB to SYSTEM PLL1 DIV6 */

    CLOCK_SetRootDivider(kCLOCK_RootAudioAhb, 1U, 2U);                    /* Set root clock freq to 800MHZ/ 2= 400MHZ*/
    CLOCK_SetRootMux(kCLOCK_RootAudioAhb, kCLOCK_AudioAhbRootmuxSysPll1); /* switch AUDIO AHB to SYSTEM PLL1 */

    CLOCK_SetRootMux(kCLOCK_RootUart4, kCLOCK_UartRootmuxSysPll1Div10); /* Set UART source to SysPLL1 Div10 80MHZ */
    CLOCK_SetRootDivider(kCLOCK_RootUart4, 1U, 1U);                     /* Set root clock to 80MHZ/ 1= 80MHZ */

    CLOCK_EnableClock(kCLOCK_Rdc);   /* Enable RDC clock */
    CLOCK_EnableClock(kCLOCK_Ocram); /* Enable Ocram clock */
    CLOCK_EnableClock(kCLOCK_Audio); /* Enable Audio clock to power on the audiomix domain*/
    
    /* The purpose to enable the following modules clock is to make sure the M7 core could work normally when A53 core
     * enters the low power status.*/
    CLOCK_EnableClock(kCLOCK_Sim_m);
    CLOCK_EnableClock(kCLOCK_Sim_main);
    CLOCK_EnableClock(kCLOCK_Sim_s);
    CLOCK_EnableClock(kCLOCK_Sim_wakeup);
    CLOCK_EnableClock(kCLOCK_Debug);
    CLOCK_EnableClock(kCLOCK_Dram);
    CLOCK_EnableClock(kCLOCK_Sec_Debug);

    /* Power up the audiomix domain by M7 core.*/
    GPC->PGC_CPU_M7_MAPPING |= 1U << GPC_PGC_CPU_M7_MAPPING_AUDIOMIX_DOMAIN_SHIFT; /* Map the audiomix domain to M7 */
    GPC->PU_PGC_SW_PUP_REQ |= 1U << GPC_PU_PGC_SW_PUP_REQ_AUDIOMIX_SW_PUP_REQ_SHIFT; /* Software request to trigger power up the domain */
    
    while(GPC->PU_PGC_SW_PUP_REQ & (1U << GPC_PU_PGC_SW_PUP_REQ_AUDIOMIX_SW_PUP_REQ_SHIFT)); /* Waiting the GPC_PU_PGC_SW_PUP_REQ_AUDIOMIX_SW_PUP_REQ bit self-cleared after power up */
    /* Do the handshake to make sure the NOC bus ready after power up the AUDIOMIX domain. */
    GPC->PU_PWRHSK |= 1U << GPC_PU_PWRHSK_GPC_AUDIOMIX_NOC_PWRDNREQN_SHIFT;
    while(!(GPC->PU_PWRHSK & (1U << GPC_PU_PWRHSK_GPC_AUDIOMIX_PWRDNACKN_SHIFT))) ;
    
    AUDIOMIX_InitAudioPll(AUDIOMIX, &g_saiPLLConfig); /* init SAI PLL run at 361267200HZ */
    /* Update core clock */
    SystemCoreClockUpdate();
}

 

 

 The read speed is too low, 33s/100M, that means only 3 Mhz/s to read the SAI RDR(n) Register

Is that  normal  or need to other configuration need to do?

Thank you in advance.

 

Labels (1)
Tags (1)
0 Kudos
Reply
2 Replies

2,149 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

SAI is designed for audio, not just for sending and receiving data, so it is normal with slow speeds.

0 Kudos
Reply

2,119 Views
Chengting
Contributor II

In iMX8MPRM.pdf,chapter 14

 • SAI1 supports to up to 8 I2S/TDM Tx lanes and 8 I2S/TDM Rx lanes at 768kHz/32-
bit

How to configure this, by our experiment, it could also result in fifo error.

Does that mean, only SAI SDMA could support that condition?

0 Kudos
Reply