imx8mp evk ov5640 dual camera support

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx8mp evk ov5640 dual camera support

176 Views
devds
Contributor III

Hello NXP Community,

Can you please let me know whether imx8mp evk, will it support two ov5640 cameras connected to two MIPI CSI in anyway ?

Thanks in Advance.

0 Kudos
Reply
2 Replies

169 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport
0 Kudos
Reply

138 Views
devds
Contributor III

Hello @Bio_TICFSL ,

Thanks for reply,

In the link you have shared seems for  i.MX 8QM MEK but my borad is imx8mp evk, anyway

Also in link shared it says to check via gstreamer commands, but presently i have only one ov5640 camera connected to either of two MIPI CSI via isi. 

If you could please confirm that imx8mp evk supports dual ov5640(connected to two MIPI CSI) (if not ov5640, let me know which one is supported) then i can check accordingly. based on this confirmation i can plan dual camera activities.

Also i'm exploring ways to port ov5640 via ISP, from this community i came to know that ov5640 via ISP is not supported, Regarding this also could you please let me know which other cameras support via ISP.

Thanks in Advance,

0 Kudos
Reply