imx8mp eARC not used strapping recommendations

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx8mp eARC not used strapping recommendations

Jump to solution
655 Views
diegoperez
Contributor II

Hi,

In the imx8mp datahseet there are recommendations about unused function. I will not use eARC function, so recommendations says:

  • VDD_EARC_1P8 tied to  ground  using a 10k resistor.
  • EARC_AUX, EARC_N_HDP, EARC_P_UTIL can be not connected

But, it is easier for my layout to leave this ball connected to 1v8 than connect to an 10k resistor to GND.

Is there a problem if VDD_EARC_1P8 is 1v8 powered and EARC_AUX, EARC_N_HDP, EARC_P_UTIL is not connected?Captura.PNG

Labels (1)
0 Kudos
1 Solution
651 Views
igorpadykov
NXP Employee
NXP Employee

Hi Diego

 

>Is there a problem if VDD_EARC_1P8 is 1v8 powered and EARC_AUX, EARC_N_HDP, EARC_P_UTIL is not connected?

 

it is ok, no problem.

 

Best regards
igor

View solution in original post

0 Kudos
1 Reply
652 Views
igorpadykov
NXP Employee
NXP Employee

Hi Diego

 

>Is there a problem if VDD_EARC_1P8 is 1v8 powered and EARC_AUX, EARC_N_HDP, EARC_P_UTIL is not connected?

 

it is ok, no problem.

 

Best regards
igor

0 Kudos