imx8mp and csi mipi speed

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx8mp and csi mipi speed

3,008 Views
arno_0
Contributor III

I attached a MIPI sensor to the imx8mp board. It uses 4 lanes and 8bit/pixel. Sensor has its own clock and it is master.

It turns out that mipi status register look fine up to a MIPI data speed of 700Mbps (each lane). If I go behind that 800 ... 1200Mbps I observe few or many (depending on speed) failure reports from MIPI_CSIS_INTSRC.

Is one of the clocks in imx8 to low? Which one is (or maybe more than one of the clocks are) responsible? I can exclude the quality of wiring/connection between sensor and board. I have two different setups, that behave in terms of this 700Mbps limit exactly the same.

Tags (3)
0 Kudos
4 Replies

2,949 Views
arno_0
Contributor III

For me MIPI seems the limit. What is it's clock, maybe it is to low in my application?

MIPI receives data and show CRC/ECC .. errror.

The ISI can handle up to 4K-res*24bpp*30fps (4k=8MPixel) = 5.76Gbps - less than 1.5Gbps with 4 lanes.

So why it shouldn't work with 1.2Gbps and 4 lanes? Maybe my clock-tree is not right? That is why I ask which clock and what frequency is used for this block.

0 Kudos

2,963 Views
arno_0
Contributor III

Thanks four your answer. Where have you find that? I don't understand - isn't the CSI referrred to operate til 1.5Gbps?

The pixeldata rate in my uses case (for ISI that is next step after CSI, right) is only about 275 MPixel/s. Nevertheless I need a 1.2Gbps on 4 lanes for that  (600MByte/s including overhead - that's why I use Byte not Pixel) - although here 1Pixel is 8bit.

This is because sensorchip processing depends on MIPI clock and there is no continuous pixel data (valid image data) transferred. So, there is some pause in between. 

So, is it possible to feed the imx8mp with that? Sorry I didn't found that clear information about processor limit.

0 Kudos

2,955 Views
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hi

 

 The detailed  information is in iMX_8M_Plus_RM_RevD

0 Kudos

2,975 Views
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hi

 

i.MX8MP:Camera ISP, 12MP res., up to 375MP/s

 

So 4 lanes the max MIPI data speed is 700Mbps (each lane)

0 Kudos