imx8mp: NPU / tensorflow-lite in new BSP (6.1) slower 3.8 vs 2.5ms

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx8mp: NPU / tensorflow-lite in new BSP (6.1) slower 3.8 vs 2.5ms

3,211件の閲覧回数
arno_0
Contributor III

For me it seems that the tensorflow lite example delegated to the NPU is getting slower.

With latest BSP (Kernel 6.1) it takes around 50% longer. Any reason?

0 件の賞賛
返信
7 返答(返信)

3,014件の閲覧回数
arno_0
Contributor III

There is an update to L6.1.1_1.0.1 - maybe it contains a fix. If you test this, let us know.

0 件の賞賛
返信

3,187件の閲覧回数
arno_0
Contributor III

Ok, found in Machine Learning User Guide:

"Known issue: Decreased performance on MobilenetV1, MobileNetV2, VGG16, VGG19, and NasNet Mobile"

But why?

 

0 件の賞賛
返信

3,174件の閲覧回数
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hi @arno_0 

Maybe the VX delegate haven't been updated to compatible with the new features.

You can use the L5.15.X and we will fix this known issue in next release.

3,026件の閲覧回数
lfant
Contributor II

@Zhiming_Liu : do you have any updates on:

1) the root cause of this performance regression

2) any potential workarounds, if kernel 6.1 needs to be used

3) timeline for a fix of the performance regression

0 件の賞賛
返信

2,880件の閲覧回数
lfant
Contributor II

I'm answering the question myself: new release (LF6.1.22_2.0.0) is out which claims to include a fix for the decreased performance (not verified yet if actually true)

@Zhiming_Liu : thanks for the support, and quick response.

0 件の賞賛
返信

3,145件の閲覧回数
lfant
Contributor II

Hello,

I will also have to use L6.1.x together with a performance-critical application using the NPU: can you please elaborate what "Maybe the VC delegate haven't been updated" exactly means? 

When will the release containing the fix that you mentioned be available?

0 件の賞賛
返信

3,165件の閲覧回数
arno_0
Contributor III
Is a mixed operation possible? So use 6.1 kernel and just the older delegates and libs?
I need the 6.1 kernel for other tthings.
0 件の賞賛
返信
An error has occurred when reading existing sub-variable "Language_PG_Configuration"; see cause exception! The type of the containing value was: extended_hash+string (lithium.coreapi.webui.template.models.NamedValueByNameTemplateModel wrapped into f.e.b.StringModel) ---- FTL stack trace ("~" means nesting-related): - Failed at: #assign redirect_lingo_page_url = web... [in template "language_macro_header.ftl" at line 173, column 1] - Reached through: #include "language_macro_header.ftl" [in template "Language_translator_Dashboard" at line 3, column 1] ----