Hello everybody,
I am working at running both A53 and M7 on an i.MX8M Plus at the same time.
Yocto-compiled Linux runs on top of A53 cores, while at the moment I am simply running MCUXpresso's hello_world demo on M7 (compiled for using TCM only).
I have configured remoteproc on Linux, and now I am perfectly able to start/stop M7 from Linux console, deploying to M7 the ELF of hello_world demo. And both (A53 and M7) work perfectly fine.
Now I am managing to fire the execution of M7 from U-Boot.
Even in this case everything is fine and I am able to start the M7 from U-Boot (deploying to M7 the BIN of hello_world demo). The problem arises when then I attempt to start Linux on A53s. The operating system crashes during boot with the following message:
[ 2.914112] remoteproc remoteproc0: imx-rproc is available
[ 2.923854] remoteproc remoteproc0: attaching to imx-rproc
[ 2.929418] Unable to handle kernel paging request at virtual address ffff80000a264fff
[ 2.937347] Mem abort info:
[ 2.940154] ESR = 0x0000000096000007
[ 2.943920] EC = 0x25: DABT (current EL), IL = 32 bits
[ 2.947769] mmc1: SDHCI controller on 30b50000.mmc [30b50000.mmc] using ADMA
[ 2.949239] SET = 0, FnV = 0
[ 2.959338] EA = 0, S1PTW = 0
[ 2.962476] FSC = 0x07: level 3 translation fault
[ 2.967354] Data abort info:
[ 2.970230] ISV = 0, ISS = 0x00000007
[ 2.974066] CM = 0, WnR = 0
[ 2.977035] swapper pgtable: 4k pages, 48-bit VAs, pgdp=0000000041d89000
[ 2.983737] [ffff80000a264fff] pgd=1000000074eee003, p4d=1000000074eee003, pud=1000000074eed003, pmd=10000000444ef003, pte=0000000000000000
[ 2.996274] Internal error: Oops: 0000000096000007 [#1] PREEMPT SMP
[ 3.002539] Modules linked in:
[ 3.005592] CPU: 2 PID: 8 Comm: kworker/u8:0 Not tainted 6.1.55+g97604c995a86 #1
[ 3.012986] Hardware name: AESYS 2319A (DT)
[ 3.016976] mmc1: host does not support reading read-only switch, assuming write-enable
[ 3.017166] Workqueue: events_unbound deferred_probe_work_func
[ 3.030991] pstate: 00000005 (nzcv daif -PAN -UAO -TCO -DIT -SSBS BTYPE=--)
[ 3.037950] pc : rproc_handle_resources.constprop.0+0x8c/0x164
[ 3.043786] lr : rproc_boot+0x304/0x580
[ 3.047621] sp : ffff800009fab9f0
[ 3.050931] x29: ffff800009fab9f0 x28: ffff000024d53a98 x27: ffff8000098bb780
[ 3.050978] mmc1: new ultra high speed SDR104 SDHC card at address 0001
[ 3.058068] x26: 0000000000000006 x25: ffffffffffffffff x24: ffff80000a265000
[ 3.058074] x23: ffff000004a1c038
[ 3.065096] mmcblk1: mmc1:0001 SD32G 28.9 GiB
[ 3.071809] x22: 0000000000000000 x21: ffff800009e1a2f0
[ 3.071814] x20: ffff000004a1c000 x19: 0000000000000000 x18: 0000000000000006
[ 3.071820] x17: 000000040044ffff x16: ffff000024cfc7e0 x15: ffffffffffffffff
[ 3.071827] x14: fff7ffffffefffff x13: ffffffffffffffff
[ 3.076558] mmcblk1: p1 p2 p3 p4
[ 3.079574] x12: fff7ffffffefffff
[ 3.079577] x11: ffffffffffffffff x10: ffffffffffffffff x9 : ffffffffffffffff
[ 3.079584] x8 : ffffffffffffffff x7 : ffffffffffffffff x6 : ffffffffffffffff
[ 3.125331] x5 : ffff000004b33000 x4 : ffff80000a265400 x3 : 00000000000003fd
[ 3.132466] x2 : 00000000ffffffff x1 : ffff80000a265003 x0 : ffff80000a265000
[ 3.139602] Call trace:
[ 3.142045] rproc_handle_resources.constprop.0+0x8c/0x164
[ 3.147532] rproc_boot+0x304/0x580
[ 3.151019] rproc_add+0xd0/0x170
[ 3.154332] imx_rproc_probe+0x464/0x5b0
[ 3.158254] platform_probe+0x68/0xc0
[ 3.161915] really_probe+0xbc/0x2dc
[ 3.165490] __driver_probe_device+0x78/0x114
[ 3.169847] driver_probe_device+0xd8/0x15c
[ 3.174030] __device_attach_driver+0xb8/0x134
[ 3.178473] bus_for_each_drv+0x80/0xdc
[ 3.182308] __device_attach+0xa0/0x1a0
[ 3.186144] device_initial_probe+0x14/0x20
[ 3.190327] bus_probe_device+0x98/0xa0
[ 3.194162] deferred_probe_work_func+0x80/0xc0
[ 3.198693] process_one_work+0x1d4/0x330
[ 3.202702] worker_thread+0x224/0x42c
[ 3.206450] kthread+0x108/0x10c
[ 3.209676] ret_from_fork+0x10/0x20
[ 3.213253] Code: 128002b3 913f6021 97ffb5f6 1400002f (b8796b00)
[ 3.219345] ---[ end trace 0000000000000000 ]---
I just suspect some troubles with memory reservation/mapping... but why does it happen only when M7 is started from U-Boot, and not if M7 is started from remoteproc?
The relevant portion of Linux DTS is the following:
&resmem {
m7_reserved: m7@75000000 {
no-map;
reg = <0 0x75000000 0 0x1000000>;
};
m7_vdev0vring0: vdev0vring0@74ff8000 {
reg = <0 0x74ff8000 0 0x8000>;
no-map;
};
m7_vdev0vring1: vdev0vring1@74ff0000 {
reg = <0 0x74ff0000 0 0x8000>;
no-map;
};
m7_vdevbuffer: vdevbuffer@74ef0000 {
compatible = "shared-dma-pool";
reg = <0 0x74ef0000 0 0x100000>;
no-map;
};
m7_rsc_table: rsc-table@74eef000 {
reg = <0 0x74eef000 0 0x1000>;
no-map;
};
m7_itcm: m7-itcm@0x7e0000 {
reg = <0 0x7e0000 0 0x20000>;
no-map;
};
m7_dtcm: m7-dtcm@0x800000 {
reg = <0 0x800000 0 0x20000>;
no-map;
};
};
/ {
imx8mp-cm7 {
compatible = "fsl,imx8mp-cm7";
rsc-da = <0x74ff8000>;
clocks = <&clk IMX8MP_CLK_M7_DIV>;
clock-names = "core";
mbox-names = "tx", "rx", "rxdb";
mboxes = <&mu 0 1
&mu 1 1
&mu 3 1>;
memory-region = <&m7_vdevbuffer>, <&m7_vdev0vring0>, <&m7_vdev0vring1>, <&m7_rsc_table>, <&m7_itcm>, <&m7_dtcm>;
status = "okay";
fsl,startup-delay-ms = <500>;
fsl,auto-boot;
};
};
/*
* ATTENTION: M7 may use IPs like below
* UART4
*/
&uart4 {
status = "disabled";
};
Any ideas?
Thanks + regards.