imx8mp: Linux 5.4.70: USB Disconnect causes exception (OOPS) in usb_hcd_check_unlink_urb()

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

imx8mp: Linux 5.4.70: USB Disconnect causes exception (OOPS) in usb_hcd_check_unlink_urb()

5,263 次查看
mahesh_hns
Contributor II

Hello,

I have a imx8mp running linux 5.4.70 connected to a USB modem. When running a test case where the USB2 is powered off (manully through linux commandline or powering the USB modem off forcibly) many times, once in a while the linux kernel throws exception as below

1577.892050] Mem abort info:
[ 1577.894844] ESR = 0x96000006
[ 1577.897897] EC = 0x25: DABT (current EL), IL = 32 bits
[ 1577.903208] SET = 0, FnV = 0
[ 1577.906259] EA = 0, S1PTW = 0
[ 1577.909400] Data abort info:
[ 1577.912279] ISV = 0, ISS = 0x00000006
[ 1577.916113] CM = 0, WnR = 0
[ 1577.919081] user pgtable: 4k pages, 48-bit VAs, pgdp=0000000058663000
[ 1577.925521] [0000000000000001] pgd=00000000586a9003, pud=00000000586ac003, pmd=0000000000000000
[ 1577.934223] Internal error: Oops: 96000006 [#1] PREEMPT SMP
[ 1577.939795] Modules linked in: mxl_moca_ctrl(O)
[ 1577.944332] CPU: 0 PID: 1503 Comm: kworker/0:0 Tainted: G W O 5.4.70-2.3.0-00011-g66b1d56-dirty #40
[ 1577.954504] Hardware name: SSMv2 Board (DT)
[ 1577.958694] Workqueue: usb_hub_wq hub_event
[ 1577.962880] pstate: 60000085 (nZCv daIf -PAN -UAO)
[ 1577.967673] pc : usb_hcd_check_unlink_urb+0x194/0x430
[ 1577.972727] lr : usb_hcd_check_unlink_urb+0x178/0x430
[ 1577.977776] sp : ffff8000123fb7c0
[ 1577.981089] x29: ffff8000123fb7d0 x28: ffff00001d2aa000
[ 1577.986404] x27: ffff00001d2a0810 x26: ffff800010ff31d8
[ 1577.991716] x25: ffff00001dae7a18 x24: 00000000ffffff94
[ 1577.997028] x23: ffff800011b09000 x22: ffff80001133b9f0
[ 1578.002340] x21: ffff800011b091a0 x20: ffff00001dae7a00
[ 1578.007651] x19: 0000000000000001 x18: 0000000000000030
[ 1578.012963] x17: 0000000000000000 x16: 0000000000000000
[ 1578.018275] x15: ffff80001187c000 x14: 3a7473694c206573
[ 1578.023587] x13: 7265766172542020 x12: 353332313a627275
[ 1578.028899] x11: 5f6b6e696c6e755f x10: 6b636568635f6463
[ 1578.034045] usb 2-1: usb_submit_urb:380 : dev->state < USB_STATE_UNAUTHENTICATED, returning -ENODEV
[ 1578.034212] x9 : 0000000000000000 x8 : 0000000000000007
[ 1578.043372] write urb submit err -19
[ 1578.048651] x7 : 00000000000285b5 x6 : 0000000000000001
[ 1578.048655] x5 : 0000000000000001 x4 : 0000000000000000
[ 1578.048659] x3 : ffff800010ff31d8 x2 : 109c0ec419c3fc00
[ 1578.048663] x1 : 109c0ec419c3fc00 x0 : ffff8000119e1a40
[ 1578.048667] Call trace:
[ 1578.048673] usb_hcd_check_unlink_urb+0x194/0x430
[ 1578.048681] xhci_urb_dequeue+0x58/0x500
[ 1578.057560] unlink1+0x44/0x188
[ 1578.057564] usb_hcd_flush_endpoint+0x1e8/0x498
[ 1578.057569] usb_disable_endpoint+0x64/0x248
[ 1578.057575] usb_disable_interface+0x64/0x100
[ 1578.068191] usb_unbind_interface+0x174/0x3d0
[ 1578.068197] device_release_driver_internal+0xf4/0x1c0
[ 1578.068201] device_release_driver+0x14/0x20
[ 1578.068207] bus_remove_device+0xcc/0x150
[ 1578.075960] device_del+0x13c/0x348
[ 1578.075964] usb_disable_device+0xac/0x2d0
[ 1578.075968] usb_disconnect+0xa4/0x3b8
[ 1578.075974] hub_port_connect+0x7c/0x740

 

After putting debug prints, it was found that the hcd->ep.urb_list sometimes has a NULL entry or an entry which, when accessed throws OOPS (perhaps freed memory, but non NULL). Has anyone faced this issue? or a similar one?

 

标签 (2)
标记 (1)
0 项奖励
回复
11 回复数

5,193 次查看
mahesh_hns
Contributor II

Thanks for the reply.

We use a custom board. The patch suggested doesn't apply to the older code baseline we are on (5.4.70_2.3.0). 

I am trying to get our changes to linux-imx-L5.15y and hit a snag with finding the latest tool chain for the same. Is there a download link for the imx-5.15 toolchain to build the linux kernel standalone?  The Linux user guide suggests building a SDK in yocto and building the tool chain that way, but I am running in to issues setting it up. Is there a download link for the tool chain to cross compile linux-5.15y?

 

0 项奖励
回复

5,181 次查看
mahesh_hns
Contributor II

Thanks for the reply.

Okay. As per the Linux User Guide, here is the procedure I followed on a Docker VM (ubuntu 20.04)

mkdir imx-yocto-bsp
cd imx-yocto-bsp
repo init -u https://github.com/nxp-imx/imx-manifest -b imx-linux-kirkstone -m imx-5.15.71-2.2.0.xml
repo sync
DISTRO=fsl-imx-xwayland MACHINE=imx8mp-lpddr4-evk source imx-setup-release.sh ./build-xwayland
bitbake core-image-minimal -c populate_sdk

docker_mradhakr@6138e6418416:/build_env/imx-yocto-bsp/build-xwayland$ bitbake core-image-minimal -c populate_sdk
Traceback (most recent call last):
File "/build_env/imx-yocto-bsp/sources/poky/bitbake/bin/bitbake", line 37, in <module>
sys.exit(bitbake_main(BitBakeConfigParameters(sys.argv),
File "/build_env/imx-yocto-bsp/sources/poky/bitbake/lib/bb/main.py", line 378, in bitbake_main
return ui_module.main(server_connection.connection, server_connection.events,
File "/build_env/imx-yocto-bsp/sources/poky/bitbake/lib/bb/ui/knotty.py", line 415, in main
params.updateToServer(server, os.environ.copy())
File "/build_env/imx-yocto-bsp/sources/poky/bitbake/lib/bb/cookerdata.py", line 75, in updateToServer
raise Exception("Unable to update the server configuration with local parameters: %s" % error)
Exception: Unable to update the server configuration with local parameters: Traceback (most recent call last):
File "/build_env/imx-yocto-bsp/sources/poky/bitbake/lib/bb/command.py", line 90, in runCommand
result = command_method(self, commandline)
File "/build_env/imx-yocto-bsp/sources/poky/bitbake/lib/bb/command.py", line 286, in updateConfig
command.cooker.updateConfigOpts(options, environment, cmdline)
File "/build_env/imx-yocto-bsp/sources/poky/bitbake/lib/bb/cooker.py", line 535, in updateConfigOpts
self.reset()
File "/build_env/imx-yocto-bsp/sources/poky/bitbake/lib/bb/cooker.py", line 1774, in reset
self.initConfigurationData()
File "/build_env/imx-yocto-bsp/sources/poky/bitbake/lib/bb/cooker.py", line 404, in initConfigurationData
self.add_filewatch(mc.getVar("__base_depends", False), self.configwatcher)
File "/build_env/imx-yocto-bsp/sources/poky/bitbake/lib/bb/cooker.py", line 313, in add_filewatch
watcher.add_watch(f, self.watchmask, quiet=False)
File "/build_env/imx-yocto-bsp/sources/poky/bitbake/lib/pyinotify.py", line 1888, in add_watch
raise WatchManagerError(err, ret_)
pyinotify.WatchManagerError: add_watch: cannot watch /build_env/imx-yocto-bsp/build-xwayland/conf WD=-1, Errno=No space left on device (ENOSPC)

doc

There is about 324G free available , I still see the above error. Do you know how I get past this error?

 

 

标记 (3)
0 项奖励
回复

5,167 次查看
AldoG
NXP TechSupport
NXP TechSupport

Hello,

searching on the web there are 2 things that you may try:

Increasing max user watches
$ sudo sysctl fs.inotify.max_user_watches=16384
https://github.com/sass/node-sass/issues/2534

clean up the Docker system
$ docker system prune
https://docs.docker.com/engine/reference/commandline/system_prune/

Best regards,
Aldo.

0 项奖励
回复

5,143 次查看
mahesh_hns
Contributor II

Thank you for the steps you mentioned. I was able to proceed with my Yocto build!

However, I am not sure itbuild the cross compilation toolchain

After  building with the above steps, the /tmp/depoy/sdk/ contains only the below

fsl-imx-xwayland-glibc-x86_64-core-image-minimal-armv8a-imx8mp-lpddr4-evk-toolchain-5.15-kirkstone.sh

When I ran it, 


You are about to install the SDK to "/disk2/mradhakr/fsl-imx-xwayland/5.15-kirkstone". Proceed [Y/n]? y
Extracting SDK..................................................................................................done
Setting it up...done
Your environment is misconfigured, you probably need to 'unset LD_LIBRARY_PATH'
but please check why this was set in the first place and that it's safe to unset.
The SDK will not operate correctly in most cases when LD_LIBRARY_PATH is set.
For more references see:
http://tldp.org/HOWTO/Program-Library-HOWTO/shared-libraries.html#AEN80
http://xahlee.info/UnixResource_dir/_/ldpath.html
/disk2/mradhakr/fsl-imx-xwayland/5.15-kirkstone/post-relocate-setup.sh: Failed to source /disk2/mradhakr/fsl-imx-xwayland/5.15-kirkstone/environment-setup-armv8a-poky-linux with status 1
SDK has been successfully set up and is ready to be used.
Each time you wish to use the SDK in a new shell session, you need to source the environment setup script e.g.
$ . /disk2/mradhakr/fsl-imx-xwayland/5.15-kirkstone/environment-setup-armv8a-poky-linux

 

Now, I was expecting aarch64-poky-linux which isn't there.  Did I use a wrong target/machine? (imx8mp-lpddr4-evk)

My intention is to build cross compilation tools (running on x86_64) to compile imx8mp linux standalone

 

0 项奖励
回复

5,116 次查看
AldoG
NXP TechSupport
NXP TechSupport

Hello,

Please try by using the following command:
$ unset LDFLAGS

Best regards,
Aldo.

0 项奖励
回复

5,110 次查看
mahesh_hns
Contributor II

Thanks,I'll try that. But my main concern is that I am not seeing the aarch64 file

 

/disk2/mradhakr/fsl-imx-xwayland/5.15-kirkstone/post-relocate-setup.sh: Failed to source /disk2/mradhakr/fsl-imx-xwayland/5.15-kirkstone/environment-setup-armv8a-poky-linux with status 1

 

The aarch64 file (mentioned in the user guide) does not get created. Am I building yocto with a wrong target machine?

0 项奖励
回复

5,098 次查看
AldoG
NXP TechSupport
NXP TechSupport

Hi,

No this should be correct, please try with the command:
$ unset LDFLAGS

And then install SDK again so it install all necessary files for standalone build.

Best regards,
Aldo.

0 项奖励
回复

5,096 次查看
mahesh_hns
Contributor II

Thanks, here is how it went.

mradhakr@gtowlnxvm17 /disk2/mradhakr/imx_5.15_SDK/toolchain $ unset LDFLAGS
mradhakr@gtowlnxvm17 /disk2/mradhakr/imx_5.15_SDK/toolchain $ unset LD_LIBRARY_PATH

mradhakr@gtowlnxvm17 /disk2/mradhakr/imx_5.15_SDK/toolchain $ ../fsl-imx-xwayland-glibc-x86_64-core-image-minimal-armv8a-imx8mp-lpddr4-evk-toolchain-5.15-kirkstone.sh
NXP i.MX Release Distro SDK installer version 5.15-kirkstone
============================================================
Enter target directory for SDK (default: /opt/fsl-imx-xwayland/5.15-kirkstone): /disk2/mradhakr/imx_5.15_SDK/toolchain
You are about to install the SDK to "/disk2/mradhakr/imx_5.15_SDK/toolchain". Proceed [Y/n]? Y
Extracting SDK..................................................................................................done
Setting it up...done
SDK has been successfully set up and is ready to be used.
Each time you wish to use the SDK in a new shell session, you need to source the environment setup script e.g.
$ . /disk2/mradhakr/imx_5.15_SDK/toolchain/environment-setup-armv8a-poky-linux


mradhakr@gtowlnxvm17 /disk2/mradhakr/imx_5.15_SDK/toolchain $ ls -la
total 40
drwxr-xr-x 3 mradhakr eng 4096 Feb 1 13:28 .
drwxr-xr-x 4 mradhakr eng 4096 Feb 1 13:26 ..
-rw-r--r-- 1 mradhakr eng 4143 Feb 1 13:27 environment-setup-armv8a-poky-linux
-rw-r--r-- 1 mradhakr eng 14027 Feb 1 13:27 site-config-armv8a-poky-linux
drwxr-xr-x 4 mradhakr eng 4096 Feb 1 13:27 sysroots
-rw-r--r-- 1 mradhakr eng 142 Feb 1 13:27 version-armv8a-poky-linux

 

Where is the environment-setup-aarch64-poky-linux , which I was looking for, to cross compile ? Is the ./fsl-imx-xwayland-glibc-x86_64-core-image-minimal-armv8a-imx8mp-lpddr4-evk-toolchain-5.15-kirkstone.sh produced by Yocto correct?

 

0 项奖励
回复

5,082 次查看
AldoG
NXP TechSupport
NXP TechSupport

Hello,

Yes it is correct, this will set the environmental variables needed for standalone compilation by using the following command:

$ source environment-setup-armv8a-poky-linux

Best regards,
Aldo.

0 项奖励
回复

5,188 次查看
AldoG
NXP TechSupport
NXP TechSupport

Hello,

Unfortunately no, we do not provide the toolchain it should be generate using Yocto, if you need help generating it do not hesitate to ask.

Best regards,
Aldo.

0 项奖励
回复

5,220 次查看
AldoG
NXP TechSupport
NXP TechSupport

Hello,

Would it be possible to try with latest Linux release?
Also, are you using your own custom board or is it an EVK?
If not, this seems like a similar issue as in this commit:
https://github.com/nxp-imx/linux-imx/commit/88d33c24076e4ec8a3251455baa69e62a7ebc539

Best regards,
Aldo.

0 项奖励
回复