imx8mn uuu Waiting for /dev/utp to appear

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx8mn uuu Waiting for /dev/utp to appear

2,468件の閲覧回数
andy9
Contributor I

Hi,

My CPU is IMX8MN, and the linux kernel version is linux-5.4.70. Use the kernel I compiled for uuu programming. The crotex-A serial port print information is as follows:

Run /linuxrc as init process
Found New UDC: ci_hdrc.0
ci_hdrc.0 0
ffs.utp0
file system registered
Mass Storage Function, version: 2009/09/11
LUN: removable file: (no medium)
run utp at /dev/usb-utp0/ep0[ 3.595243] read descriptors

.
uuu fastboot client 1.0.0 [b[ 3.598887] read strings
uilt Dec 16 2020 14:04:17]
Start init usb
write string
Start handle command
uuc /dev/utp
uuc 0.6 [built Dec 16 2020 14:04:17]
UTP: Waiting for /dev/utp to appear

Then it crashed。

CMD window information is as follows:

E:\ubuntu-ssh\imx8mn\linux5.4.70>uuu -v uuu.auto
uuu (Universal Update Utility) for nxp imx chips -- libuuu_1.4.72-0-g8e9e189

Build in config:
Pctl Chip Vid Pid BcdVersion
==================================================
SDPS: MX8QXP 0x1fc9 0x012f [0x0002..0xffff]
SDPS: MX8QM 0x1fc9 0x0129 [0x0002..0xffff]
SDPS: MX8DXL 0x1fc9 0x0147
SDPS: MX28 0x15a2 0x004f
SDPS: MX815 0x1fc9 0x013e
SDPS: MX865 0x1fc9 0x0146
SDP: MX7D 0x15a2 0x0076
SDP: MX6Q 0x15a2 0x0054
SDP: MX6D 0x15a2 0x0061
SDP: MX6SL 0x15a2 0x0063
SDP: MX6SX 0x15a2 0x0071
SDP: MX6UL 0x15a2 0x007d
SDP: MX6ULL 0x15a2 0x0080
SDP: MX6SLL 0x1fc9 0x0128
SDP: MX7ULP 0x1fc9 0x0126
SDP: MXRT106X 0x1fc9 0x0135
SDP: MX8MM 0x1fc9 0x0134
SDP: MX8MQ 0x1fc9 0x012b
SDPU: SPL 0x0525 0xb4a4 [0x0000..0x04ff]
SDPV: SPL1 0x0525 0xb4a4 [0x0500..0x9998]
SDPU: SPL 0x0525 0xb4a4 [0x9999..0x9999]
SDPU: SPL 0x3016 0x1001 [0x0000..0x04ff]
SDPV: SPL1 0x3016 0x1001 [0x0500..0x9998]
FBK: 0x066f 0x9afe
FBK: 0x066f 0x9bff
FB: 0x0525 0xa4a5
FB: 0x18d1 0x0d02
FB: 0x3016 0x0001
Wait for Known USB Device Appear...
New USB Device Attached at 2:2
2:2>Start Cmd:SDPS: boot -f flash.bin
100%2:2>Okay (3.087s)
New USB Device Attached at 2:2
2:2>Start Cmd:FB: ucmd setenv fastboot_dev mmc
2:2>Okay (0.016s)
2:2>Start Cmd:FB: ucmd setenv mmcdev ${emmc_dev}
2:2>Okay (0.197s)
2:2>Start Cmd:FB: flash bootloader flash.bin
0x400000002:2>Okay (0.226s)
2:2>Start Cmd:FB: ucmd if env exists emmc_ack; then ; else setenv emmc_ack 0; fi;
2:2>Okay (0.019s)
2:2>Start Cmd:FB: ucmd setenv emmc_cmd mmc partconf ${emmc_dev} ${emmc_ack} 1 0
2:2>Okay (0.006s)
2:2>Start Cmd:FB: ucmd if test "${emmc_skip_fb}" != "yes"; then run emmc_cmd; fi
2:2>Okay (0.007s)
2:2>Start Cmd:FB: ucmd setenv emmc_cmd mmc bootbus ${emmc_dev} 2 2 1;
2:2>Okay (0.005s)
2:2>Start Cmd:FB: ucmd if test "${emmc_skip_fb}" != "yes"; then run emmc_cmd; fi
2:2>Okay (0.01s)
2:2>Start Cmd:FB: ucmd setenv fastboot_buffer ${loadaddr}
2:2>Okay (0.008s)
2:2>Start Cmd:FB: download -f Image
2:2>Okay (0.748s)
2:2>Start Cmd:FB: ucmd setenv fastboot_buffer ${fdt_addr}
2:2>Okay (0.008s)
2:2>Start Cmd:FB: download -f imx8mn-ddr4-evk.dtb
2:2>Okay (0.013s)
2:2>Start Cmd:FB: ucmd setenv fastboot_buffer ${initrd_addr}
2:2>Okay (0.007s)
2:2>Start Cmd:FB: download -f fsl-image-mfgtool-initramfs-imx_mfgtools.cpio.gz.u-boot
2:2>Okay (0.377s)
2:2>Start Cmd:FB: acmd ${kboot} ${loadaddr} ${initrd_addr} ${fdt_addr}
2:2>Okay (0.003s)

 

How to solve this problem?

0 件の賞賛
返信
3 返答(返信)

2,324件の閲覧回数
imx8-mdt
Contributor I

Hi Andy

Have you fixed this issue?

I have the same problem with uuu to download to my imx8mm EVK?

I also use the  linux5.4 kernel , can't find CONFIG_FSL_UTP either.

It can't enter into FBK mode

 

0 件の賞賛
返信

2,464件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi yongqiang

 

had board passed ddr test, if not first recommended to run ddr test (also use RPA tool) and rebuild image

as described in ddr test documentation

https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX-8M-Family-DDR-Tool-Release/ta-p/110...

 

Best regards
igor

0 件の賞賛
返信

2,456件の閲覧回数
andy9
Contributor I

I have tested it, Calibration is successful, and the "ddr4_timing.c" file is also replaced. It's still stuck there now.

①、When I use the "uuu -lsusb" command, I found that imx8mn has been in the FB state and did not enter the FBK mode.

②、In the linux5.4 kernel, neither the CONFIG_FSL_UTP configuration item nor the "kernel/drivers/usb/gadget/function/fsl_updater.c" file was found. This is used to upgrade in imx7d-linux4.1.15. Does imx8mn-linux5.4 need this file? Provide a patch if need,Please.

0 件の賞賛
返信