imx8mn no network messages in sleep mode

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx8mn no network messages in sleep mode

1,324件の閲覧回数
mudherp
Contributor IV

Hi

We have the tcp/ip stack up and running by default on our ui board that uses the imx8mn.
We put the board to sleep using the following command:

echo "s2idle" > /sys/power/mem_sleep
echo mem > /sys/power/state

After we have issued the command we have monitored using wireshark the the router send an ARP message to the ui board. But the ui board does not respond to the arp message.

From the above the router sends ARP message to the ui board for at over 10 minutes. Eventually the router removes the ui board from it attached devices.

Hence if we ping the ui board it is un-reachable.

So is their a way to keep the ip stack alive when the imx8mn is asleep?

0 件の賞賛
返信
4 返答(返信)

1,293件の閲覧回数
opedis
Contributor III

There is no way to do that. 

Only way is using Wake-on-LAN ( WoL) . 

0 件の賞賛
返信

1,263件の閲覧回数
mudherp
Contributor IV

Please tell me how Wake-on-LAN ( WoL) works and how do i enable it for imx8mn-evk

 

0 件の賞賛
返信

1,277件の閲覧回数
mudherp
Contributor IV

Please tell me how Wake-on-LAN ( WoL) works and how do i enable it for imx8mn-evk

0 件の賞賛
返信

1,309件の閲覧回数
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hi @mudherp 

It's hard to realize this feature, need to modify much frameworks if we add this.

You can contact SE team for this.

Best Regards

Zhiming

0 件の賞賛
返信