imx8mn flashing a image after bitbake

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx8mn flashing a image after bitbake

2,716件の閲覧回数
shai_b
Senior Contributor II

dear team,

My customer has tried to flash the images that were created from the bitbake using uuu tool.

Tried two commands:

sudo uuu -b emmc_all imx-boot-imx8mn-ddr4-evk-sd.bin-flash_ddr4_evk imx-image-core-imx8mn-ddr4-evk.wic.bz2

sudo uuu -b emmc_all imx-boot-imx8mn-ddr4-evk-sd.bin-flash_ddr4_evk imx-image-core-imx8mn-ddr4-evk.tar.bz2

 

in the debug console of IMX8 I see the following:

 

it any key to stop autoboot:  0

## Checking Image at 43800000 ...

Unknown image format!

Run fastboot ...

 

Can you please advise what exactly am I doing wrong?

Secondly, if you could explain a bit about each file inside the deploy folder (see attached log file)?

Thanks in advance 

KR,

Shai

ラベル(2)
タグ(1)
0 件の賞賛
返信
3 返答(返信)

2,710件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

did the customer try the demo images? did their board boot up demo images successfully?

 

0 件の賞賛
返信

2,705件の閲覧回数
shai_b
Senior Contributor II

Hi @joanxie,

No, the UUU did not flash due to the following error: 

Unknown image format!

Can you please advise if the commands are correct (for flashing the imaging into the emmc)?

sudo uuu -b emmc_all imx-boot-imx8mn-ddr4-evk-sd.bin-flash_ddr4_evk imx-image-core-imx8mn-ddr4-evk.tar.bz2/*

also, can you please explain why there are so many files in the deploy folder and which one if the final "bootloader"?

Waiting for your feedback, Thanks a lot

KR,

Shai 

0 件の賞賛
返信

2,699件の閲覧回数
khang_letruong
Senior Contributor III

Hi @shai_b ,

You can add option -v to see the progress of the flashing :

sudo uuu -v -b emmc_all imx-boot-imx8mn-ddr4-evk-sd.bin-flash_ddr4_evk imx-image-core-imx8mn-ddr4-evk.tar.bz2

And sometimes, flashing issues are caused by the bad-quality USB cable.

Best Regards,
Khang

0 件の賞賛
返信