imx8mn boot from boot0 and write to boot1.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx8mn boot from boot0 and write to boot1.

1,295件の閲覧回数
liza_mary
Contributor I

Hi

I am using an imx 8m nano evk. I need to have the bootloader in the boot partitions of emmc. Initially it should boot from boot0 (boot partition 1) and write to boot1 (boot partition 2).The next time it should boot from boot1 and update to boot0. How can I handle this in the uuu script?

Really appreciate any help.

Thanks !

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,266件の閲覧回数
Zhiming_Liu
NXP TechSupport
NXP TechSupport

The uuu can't support such function, this needs you change the uboot source code and uuu code.We don't have such solution at present.

0 件の賞賛
返信

1,254件の閲覧回数
liza_mary
Contributor I

Thanks for your reply!

I think, I managed to write to both boot partitions. Now I need to set an environment variable and save it. But the saveenv doesn't work from uuu script. 

0 件の賞賛
返信