imx8mn boot from boot0 and write to boot1.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

imx8mn boot from boot0 and write to boot1.

1,380 次查看
liza_mary
Contributor I

Hi

I am using an imx 8m nano evk. I need to have the bootloader in the boot partitions of emmc. Initially it should boot from boot0 (boot partition 1) and write to boot1 (boot partition 2).The next time it should boot from boot1 and update to boot0. How can I handle this in the uuu script?

Really appreciate any help.

Thanks !

标签 (1)
0 项奖励
回复
2 回复数

1,351 次查看
Zhiming_Liu
NXP TechSupport
NXP TechSupport

The uuu can't support such function, this needs you change the uboot source code and uuu code.We don't have such solution at present.

0 项奖励
回复

1,339 次查看
liza_mary
Contributor I

Thanks for your reply!

I think, I managed to write to both boot partitions. Now I need to set an environment variable and save it. But the saveenv doesn't work from uuu script. 

0 项奖励
回复